Skip to main content
Robot arm with glowing circuit patterns against a dark background with blue light effects
産業用人工知能

SiemensはIndustrial AI革命を加速させている

AIは、前世紀を電気が変革したように、今世紀を変革するでしょう。私たちは、Design and Engineeringから運用に至るまで、物理的な世界全体にわたりAIを適用することで、お客様がアイデアをより迅速に、より高品質かつ効率的に現実世界での成果へと結びつけられるよう支援します。

An automation engineer working in a high-tech facility, viewing a digital AI robot assistant overlay on a screen alongside technical code and 3D CAD models.

Just launched: Eigen Engineering Agent

At Hannover Messe, Siemens unveiled the Eigen Engineering Agent – moving industrial AI from assistance to autonomous execution.

Siemens Xcelerator

Explore our AI products

We combine decades of industrial data, deep domain expertise and advanced AI to help customers move faster across the entire lifecycle — from engineering and design to operations. Through Siemens Xcelerator, we make trusted industrial AI accessible to all. 

Technology

What is industrial AI?

Industrial AI is AI purpose-built for the real world: The factories, buildings, trains, power grids, and hospitals that keep our economies running. Unlike consumer AI, industrial AI must work in environments where reliability, safety, and precision are critical priorities.

A designer uses a VR headset to interact with a generative design simulation

AI glossary

This glossary of the most important key terms can help broaden your understanding and delve deeper into this fascinating world.

This photo is decorative

Industrial AI and sustainability

This new report explores how AI is helping organizations realize their sustainability goals. It provides an in-depth analysis of the current and projected impact of industrial AI accelerating transformative change.

Siemens Xcelerator logo with an image of two men in the back

AI学習ハブ

AIと機械学習について深く理解しましょう。当社のトレーニングプログラムは、各分野でイノベーションを推進するために必要な知見とツールを習得できるよう設計されています。

Industries

The impact of AI on industry and infrastructure

Through technology, partnerships, and customer stories across manufacturing, buildings, transportation, grids, and AI infrastructure, we'll show how Siemens is accelerating Industrial AI and delivering real-world impact with customers and partners.

30% Reduced cooling costs in data centers

Optimize temperature management with AI-powered cooling to minimize manual intervention. This enhances efficiency and supports more sustainable data center operations by lowering energy consumption.

50% Reduced manual engineering for hydrogen plants

For hydrogen plants. Streamline plant design and engineering using generative AI. Reduce project timelines from months to weeks, enabling you to scale up green hydrogen production faster and more efficiently.

9% Improved energy efficiency in commercial buildings

Modernize outdated systems with AI-enabled edge controllers. Leverage real-time data to automate building optimization, breaking down data silos and making operations more affordable and sustainable.

Industrial AI in practice

Across manufacturing, energy, and buildings, Siemens industrial AI is generating measurable results in throughput, efficiency, cost, and uptime. These are deployed systems, in operating facilities, with outcomes that can be counted.

The image shows a digital twin composer interface with various tools and options displayed on a computer screen.

PepsiCo deployed Siemens Digital Twin Composer to simulate and optimize production line changes before any physical modifications. This led to a 20% increase in throughput at a Gatorade facility within three months, while reducing capital expenditure by 10–15% by uncovering hidden capacity.

The Mecalux and Siemens robotized picking system in action.

The new AI-powered robotized picking system is the result of a solid partnership between Mecalux and Siemens, combining knowledge and experience from both companies in industrial AI technology.

siemens-industrial-copilot-640x360

The Siemens Industrial Copilot is our generative AI assistant that empowers people across the value chain. It simplifies complex tasks like code generation and fault diagnostics through natural language, helping human experts focus on innovation and high-value problem-solving.

相互接続されたデジタルシステムと持続可能な農業技術を組み合わせたスマート農業技術

An innovative vertical farm in Dubai – among the largest in the world – is using Siemens technology to push new food production solutions to their fullest potential.

People in the loop

While industrial AI excels at data processing and automation, humans provide the accountability and contextual judgment to navigate real-world nuances. These three stories show how experts use AI to drive safety, efficiency, and continuous improvement.

Engineer talking through a radio

DAIRY MAINTENANCE MANAGER

A manager at Sachsenmilch used Senseye AI to find a pump failure weeks early. This let the team fix it during a planned stop, saving a six-figure sum and preventing the loss of thousands of liters of milk.

A man standing with his arms crossed, wearing safety gear

WATER UTILITY OPERATOR

Operators in Spain use SIWA Leak Finder to catch leaks as small as 0.2 liters per second. By pinpointing 10,000 events, they dispatch crews with precision, saving water and lowering costs for the community.

Simon and Victor from VA SYD smiling for the camera

WATER DEVELOPMENT ENGINEER

At VA SYD, engineers trained AI to monitor 2,000 km of pipe. It caught tiny leaks that sensors missed, cutting water loss from 10% to 8% and preventing major bursts before they could disrupt the city's supply.

A statue of a human on the right with the words, 'Human and AI: Mind, Machines, and the Gradient Descent.'

PODCAST SERIES

Human & AI

Our AI Lab presents podcast filled with the voices of those who re raising awareness for the potential of AI across Siemens.

OUR PERSPECTIVE

Siemens at CES 2026

Siemens demonstrated its integrated AI approach at CES 2026, showing how intelligence moves through a unified stack from engineering models to production data, edge inference to cloud deployment. One platform. Every industrial context. No reinvention required.

Roland Busch, CEO Siemens, and Jensen Huang, CEO NVDIA, shaking hands at CES 2026

Join us for the industrial AI revolution

Unlock the full potential of Industrial AI by uniting every layer required for true data intelligence.