Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser
Largest order: Siemens is building ICE 4 trains for Deutsche Bahn
In May 2011, the German national railway company concluded a framework agreement with Siemens Mobility for up to 300 trainsets. At this time the largest train contract that Siemens has ever won in its corporate history.

The ICE 4 sets new standards in intercity traffic. A unique train concept has been developed, that means it can be individually adapted to the requirements of various transport tasks. The modular drive concept is based on independent Powercars with identical traction technology, resulting in more flexibility than ever before. High operational availability is guaranteed by a large number of reliable systems with high redundancy.

All in all, DB will be receiving 1,511 cars with which it can configure 50 12-car, 50 13-car and 37 7-car trainsets. 

In addition, Deutsche Bahn has awarded Siemens Mobility a contract for the revision of 40 ICE 4 trains. 
Press Release19 March 2024

Billion-euro project completed on time: ICE 4 fleet now complete

Press Release19 January 2021

Siemens Mobility awarded service contract for ICE 4 trains

Press Release17 July 2019

Deutsche Bahn resumes acceptance
of ICE 4 trains 

Press Pictures

Largest order - Siemens is building ICE 4 trains for Deutsche Bahn

All in all, DB will be receiving 1,511 cars with which it can configure 50 12-car, 50 13-car and 37 7-car trainsets. DB will keep two end cars in reserve. The 12-car and 13-car trainsets will be operated in Germany, Austria and Switzerland. The shorter 7-car trains are planned for use in Germany and Austria.

Largest order - Siemens is building ICE 4 trains for Deutsche Bahn

All in all, DB will be receiving 1,511 cars with which it can configure 50 12-car, 50 13-car and 37 7-car trainsets. DB will keep two end cars in reserve. The 12-car and 13-car trainsets will be operated in Germany, Austria and Switzerland. The shorter 7-car trains are planned for use in Germany and Austria.

Videos: The ICE 4 - the new backbone of Deutsche Bahn's long-distance network 

Video Player is loading.
Current Time 0:00
Duration 0:00
Loaded: 0%
Stream Type LIVE
Remaining Time 0:00
 
1x
    • Chapters
    • descriptions off, selected
    • captions off, selected
      Video Player is loading.
      Current Time 0:00
      Duration 0:00
      Loaded: 0%
      Stream Type LIVE
      Remaining Time 0:00
       
      1x
        • Chapters
        • descriptions off, selected
        • captions off, selected

          Further Information

          Event Pictures

          Deutsche Bahn honors Siemens as most innovative supplier

          Deutsche Bahn honored Siemens today as its most innovative supplier. The Supplier Innovation Award was presented by Rüdiger Grube, CEO of Deutsche Bahn (DB), for the new Intercity ICE 4. Siemens was recognized for its development of a completely new vehicle concept that offers great operating flexibility. With this concept, DB can easily adapt to changing route requirements and passenger needs over the train's entire lifecycle.
          In the picture from left to right: Jochen Eickholt, CEO Siemens Mobility Division; Sabrina Soussan, CEO Siemens Business Unit Mainline Transport; Rüdiger Grube, CEO of Deutsche Bahn (DB), and Martin Offer, Project Manager ICE 4 Siemens Mobility Division.

          Premiere in Berlin: The ICE 4 is here!

          The 12-car ICE 4 has a top speed of 250 kilometers an hour and a length of 346 meters. It offers a total of 830 seats, 205 in First Class and 625 in Second Class. The train's low weight and optimized aerodynamic design reduce energy consumption per seat by 22 percent compared to the ICE 1. The innovative traction concept with so-called power cars allows flexible configuration of the trains.

          Contact

          Eva Haupenthal

          Siemens Mobility GmbH

          +49 152 01654597

          Link to this page
          www.siemens.com/press/ice4