Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser
Type X Metro Trains for Vienna
Wiener Linien commissioned Siemens at the end of 2017 with the delivery of 34 fully automated metro trains. The contract also includes the maintenance of the trains for a period of 24 years and an option for an additional eleven trains. The "X cars" will be operated fully automated on the new U5 line in Vienna beginning in 2024. The trains can also operate semi-automated or manually on previously existing lines. Delivery of the trains is scheduled to begin in mid-2020 and to be completed by 2030. The trains will be manufactured at the Siemens factory in Vienna.

Press Pictures

First painted car body presented for the new Vienna metro 

The first painted car body for the new Vienna metro was presented today together with the public transport operator Wiener Linien at the Siemens Mobility plant in the Austrian capital. The trains are the city’s third metro generation supplied by Siemens and are named “X cars.” The first pre-series train is scheduled to be delivered in mid-2020. A total of 34 six-car trainsets are to be built. Wiener Linien also secured an option for an additional eleven trains. The trains are designed for fully automatic operation as well as operation with a driver. Plans call for them to be used fully automatically on the city’s new Line U5, which is currently under construction, and with drivers on Wiener Linien’s Lines U1 to U4. 

From left to right: Günter Steinbauer, Wiener Linien Managing Director; Ulli Sima, Vienna's City Councilor for Public Transport ; Albrecht Neumann, CEO of Rolling Stock at Siemens Mobility

First painted car body presented for the new Vienna metro 

The first painted car body for the new Vienna metro was presented today together with the public transport operator Wiener Linien at the Siemens Mobility plant in the Austrian capital. The trains are the city’s third metro generation supplied by Siemens and are named “X cars.” The first pre-series train is scheduled to be delivered in mid-2020. A total of 34 six-car trainsets are to be built. Wiener Linien also secured an option for an additional eleven trains. The trains are designed for fully automatic operation as well as operation with a driver. Plans call for them to be used fully automatically on the city’s new Line U5, which is currently under construction, and with drivers on Wiener Linien’s Lines U1 to U4. 

Infographics

Type X Metro Trains for Vienna

Siemens is manufacturing 34 six-car metro trains for Wiener Linien.

Video

Video Player is loading.
Current Time 0:00
Duration 0:00
Loaded: 0%
Stream Type LIVE
Remaining Time 0:00
 
1x
    • Chapters
    • descriptions off, selected
    • captions off, selected

      Siemens to build 34 fully automated metro trains for Vienna 

      Wiener Linien commissioned Siemens at the end of 2017 with the delivery of 34 fully automated metro trains. The contract also includes the maintenance of the trains for a period of 24 years and an option for an additional eleven trains. The “X cars” will be operated fully automatically on the new U5 line in Vienna beginning in 2024. The trains can also operate semi-automatically or manually on previously existing lines. Delivery of the trains is scheduled to begin in mid-2020 and to be completed by 2030. The trains will be manufactured at the Siemens factory in Vienna.                                         

      Further Information

      Contact

      Eva Haupenthal

      Siemens Mobility GmbH

      +49 152 01654597 

      Link to this page
      www.siemens.com/press/x-vienna