Skip to main content

Investing in carbon capture technologies

Achieving net-zero by 2050 will involve ongoing removal and storage of CO₂ emissions and the use of negative emissions technologies (NET) to recapture emitted greenhouse gases

The need for diverse innovation in accelerating climate

NOVEMBER 2022

Throughout recent assessments, it’s evident that the countries that signed the Paris Climate Agreement have not managed to cut their emissions enough to meet its targets. The strategies employed to date by governments, relying heavily on more renewable energy and fewer carbon consumption, are not enough.

While the physical reduction of CO₂ emissions remains the highest priority, to help achieve net-zero goals CO₂ will also need to be removed from the atmosphere on a large scale and stored or eliminated. Even if we do reach net-zero by 2050, we will need to continue removing historic CO₂ emissions from the atmosphere in order to avoid future warming. According to the World Resources Institute scientists predict that up to 10 Gigatonnes (Gt) of CO₂ will need to be removed annually from the atmosphere by 2050, with removal capacity increasing to 20 Gt CO₂ per year by 2100. To support this removal and storage of CO₂ emissions from the atmosphere – known as carbon capture and storage (CCS) – agile innovations are needed in negative emissions technologies (NET) to recapture previously emitted greenhouse gases.

The image shows a digital twin concept with a person in a virtual environment interacting with digital objects.

With scientists in agreement, the market is emerging to help make the NET ecosystem come to life. According to the Net Zero Stocktake 2022, more than one-third (702) of world’s largest publicly traded companies now have net-zero targets, up from one-fifth (417) in December 2020 establishing a fast-growing need for an expansion of carbon credits but also for measuring and reporting progress to ensure transparency and accountability.

Time for action: Scaling NET

A person is standing in front of a large screen displaying a graph with a red line.

While NET has the potential to help accelerate climate action, to effectively scale this industry, action is required by governments, investors, and industrial players alike. Government funding has emerged to support breakthrough technologies, such as the EU Innovation Fund for a wide range of clean technologies, and the U.S.’s recent Inflation Reduction Act (IRA) which offers enhanced tax credits for the permanent sequestration of CO₂. However, gathering full-force support in maturing NET technologies requires additional private-sector financing as well as ecosystem expertise to effectively bring these solutions to the market. And timing is also crucial – these technologies need to mature at a break-neck pace to meet the large-scale need to be impactful.

Funding these growth companies goes beyond capital. Investment partners must also offer the necessary industry knowledge and an internationally established market footprint to help mature emerging technologies as they navigate many risks, including reliability and scalability, to achieve market-readiness.

SFS as strategic enabler of NET impact​

As an experienced investing partner in decarbonization technologies across a wide variety of industries, Siemens Financial Services (SFS) is joining several forward-looking players in proactively investing in companies developing NET. Backed by the Siemens industrial businesses, SFS can offer the strategic solutions that address the many challenges growth companies face – start-up capital, ecosystem access and development time.

In this way, SFS is an ideal partner for NET companies, providing more than money to help multiply impact. As a global technology leader, Siemens is one of the few companies in the world that has a proven track record as a key enabler of decarbonization from renewable energy to smart infrastructure and efficient manufacturing. Siemens can also provide companies access to technologies such as digital twin and high-end process modelling necessary to help pilot projects for larger-scale use.

The image shows a person standing in front of a large, colorful mural with a mix of abstract and realistic elements.
As climate action is currently lagging, we need to consider all options to accelerate the path to net-zero. We know that removing CO₂ from the atmosphere will be vital to meeting net-zero targets, and ultimately to reversing climate change. SFS is proud to be supporting emerging NET technologies both financially and through our expertise.
Steffen Grosse, CEO of Equity Finance, SFS

Customer reference: CarbonCapture, Inc.

SFS has recently made a strategic investment in CarbonCapture, Inc., a leading climate technology company in the United States. The company specializes in direct air capture (DAC) systems designed to remove CO₂ from the atmosphere.

Recognizing the pressing need for large-scale CO₂ removal, CarbonCapture, Inc. has developed DAC machines utilizing a modular, scalable, and highly-upgradable system architecture. This innovative approach enables mass manufacturing and facilitates the integration of rapidly advancing sorbent technologies.

Customer reference: Neustark​

Additionally, SFS made an early-stage investment in Neustark, which developed a solution that uses the carbonization of recyclable demolished concrete – the world’s largest waste stream – to permanently remove and store CO₂ from the atmosphere, creating negative emissions. Headquartered in Switzerland and currently operating throughout Europe, Neustark aims to scale its operations globally and reach its goal to remove one million tons of CO₂ in 2030, and beyond that. Neustark’s technology integrates seamlessly into the current concrete recycling process and helps local concrete recyclers answer customer demand and generate additional income with low-carbon building materials.SFS believes in technology with purpose. We understand the role that both capital and ecosystem knowledge play in forming new markets, helping to pioneer strategic partnerships to scale for maximum sustainable impact.

Neustark CO2 tank and carbonization factory with demolished concrete.