Skip to main content
Fair

International Industrial Fair 2026

October 6 – 9, 2026 | Pavilion F, Booth 200 - National Center for Industry 4.0 | BVV Brno

Keyvisual: Siemens brings AI to the physical world with Eigen Engineering Agent<br/>

Benefits of software-based manufacturing.

At this year’s International Engineering Fair, we introduced you to the benefits of manufacturing where software plays a key role. You learned how artificial intelligence can improve processes, increase efficiency, and give you a competitive edge. We also advised you on how to make the most of simulation and virtual reality, and how to ensure cyber-secure manufacturing.

Thank you for visiting us and for all the inspiring encounters.

What Did We Showcase at MSV 2026?

Webinar: Meet Eigen Engineering Agent - the AI agent in TIA Portal

Eigen Engineering Agent

An AI system integrated into the TIA Portal platform that autonomously plans, executes, and validates engineering tasks.

Optimize MyProgramming /3D Scanner

Sinumerik ONE

The exhibit featured the powerful, compatible, and modern Sinumerik ONE control system with a digital twin. This custom-designed solution also allows users to test new CNC programs and fully optimize them in a virtual environment.

Low voltage conditon monitoing icon

Condition monitoring

The new generation of Siemens Condition Monitoring solutions, integrated into the Industrial Edge platform, enables secure data processing directly in the manufacturing environment.

Visual Cybersecurity for Industry Network Security

Cybersecurity and NIS2

Given the growing threats, cybersecurity in industry is currently a highly important issue. Regulatory authorities require industries and businesses to strengthen the protection of their operations and customers.

Graafinen esitys tietokoneen työpöydästä, johon on yhdistetty sovelluksia ja laitteita.

Industrial Edge

Industrial Edge brings real-time insights and intelligent data processing straight to your production facilities.

Senseye Predictive Maintenance

Senseye predictive maintenance

A scalable predictive maintenance approach that helps manufacturers anticipate risk, focus effort where it matters and improve asset reliability across operations.

Retrofit and Modernization Services Keyvisual

Retrofit and modernization

Siemens retrofits extend machine tool life with advanced SINUMERIK CNC, improving productivity, reducing downtime and enabling data-driven performance.

A person seen from behind is near a white work surface, a monitor with a SIEMENS machine-simulation interface, and a plant.

Run MyVirtual Machine

Run MyVirtual Machine is the digital twin platform for SINUMERIK CNC, supporting programming, verification and training with high‑fidelity simulation.

Two people wearing safety glasses looking at a computer monitor.

SCALANCE

Portfolio of industrial network components. SCALANCE XR300-500 for high-performance networks. SCALANCE XFM-200 for shallow-mount control cabinets. SCALANCE S605 for firewalling and remote management of even the smallest machines.

A person points at a tank-control schematic on an industrial control console beside five buttons.

SIMATIC Ident – RF1000

Identify machine operators using an existing PKI card. Flexible integration with HMI panels, SCADA, and DCS systems.

An engineer working at a desk with multiple monitors displaying 3D simulation models and data charts.

Simcenter

Analyze fully detailed CAD assemblies in just a few minutes by eliminating the need to simplify geometry and create meshes.

Immersive Engineering in action, reviewing a 3D design in XR with Designcenter NX.

CAD Software Designcenter

A modern, integrated solution for product development that combines design, simulation, and manufacturing processes into a single digital environment and supports innovation at every stage of development.

Computer screen displaying system requirements for NX CAM software with processor, RAM, and graphics specifications.

NX CAM

Transform your entire parts manufacturing process using a single, comprehensive computer-aided manufacturing (CAM) software solution.

Person wearing VR headset in futuristic environment with holographic displays

Immersive Engineering

Immersive Engineering is transforming the way products are developed by combining augmented, virtual, and mixed reality into a single immersive engineering environment.

A flow diagram links a white cloud and server racks via green paths, robotics, a conveyor belt, and a purple OT shield.

SINEC Secure Connect

A platform for communication and remote access based on Zero Trust principles and optimized for the industrial sector (OT).

A blue scene shows two figures; one wears purple and a hat, with network graphic above, clock, and magnifying glass in a box.

SINEC Security Inspector

A tool for one-time and recurring scans of OT assets for malware and vulnerabilities. Suitable for both suppliers and end operators.

A person in purple clothing is on the left, and a hat-wearing person in purple is on the right; a display shows a colored eye-and-circular motif and a clock- or gauge-like circle against a dark background with blue or teal technical-looking lines.

SINEC Security Monitor

An intrusion detection system that enables passive, continuous monitoring of OT networks during production for maximum transparency and early threat detection. Also verified for use in SIMATIC PCS7 process installations.

A purple shield with a circuit-like pattern appears alongside a bar chart, checked document, clock, checked padlock, line graph, and magnifying glass.

SINEC Security Guard

Try out vulnerability management software. There's nothing to install—just import your assets and start testing!

A bearded man with dark hair and glasses holds a laptop beside a screen with panels, lightbulbs, and connected nodes.

SINEC Advanced Network Suite

Design your networks using professional software without having to install anything. From designing networks using pre-made diagrams, to segmenting them with firewalls and VLANs, to calculating network parameters and protocols.

Key Visual Remote Access for Teleservice (RGB)

Remote management – SINEMA remote connect

We offer secure remote communication solutions for the manufacturing and processing industries that meet the cybersecurity requirements of the NIS2 Directive.

Xbot motion cropped

Showcase of planar motor system

Transport units levitate above the modular stator plates. Due to this design, the system operates entirely without mechanical contact, wear, or lubrication. The exhibit includes the SIMATIC S7-1500T Station Management library too.

DigiStand visual MSV2026 webpage

DigiStand

DigiStand is a training station based on the SINUMERIK ONE control system and a digital twin of a machine tool.

CNC machine tool paired with its digital twin wireframe rendering on dark background

Digital Twin

A demonstration of the digital twin of the VOSA modular CNC machine by VOPSS Řepeč s.r.o., showcasing simulation, virtual validation, and machine optimization capabilities in a digital environment before commissioning.

Cybersecurity

Cybersecurity and Resilience Testing

At the National Center for Industry 4.0 booth, you tested your production’s resilience to cyber threats. You gained insight into potential vulnerabilities and recommendations to improve industrial system security.

BVV Brno, Pavilion F, booth 200, 06. 10. - 09. 10. 2026

Siemens participated in the trade show as a partner of the National Industry 4.0 Center.

For more information on participating in the International Engineering Fair 2006, please visit the website of the National Center for Industry 4.0.