Skip to main content
Industrial AI

Industrial AI in manufacturing

By: U.S. Corporate Communications

Artificial intelligence (AI) has already demonstrated that it can analyze information, uncover patterns and make recommendations. Industrial AI faces a tougher test: Can it turn those insights into measurable improvements on the factory floor?

The National Institute of Standards and Technology’s (NIST) 2026 work on AI for manufacturing reflects that this challenge. Alongside AI's potential for greater productivity and resilience, it identifies technical complexity, ROI uncertainty, interoperability, and reliable deployment among the challenges standing between experimentation and widespread manufacturing use.

At Siemens, we combine AI capabilities with deep knowledge of industrial equipment, automation and engineering. This enables us to help customers to apply AI across real production, maintenance, and engineering workflows.

For U.S. manufacturers, AI creates value when it solves a measurable operational problem, works inside mixed technology environments, and earns enough trust to influence physical operations. Operations must perform better because of it.

Where should manufacturers deploy Industrial AI first for measurable value?

Manufacturers should start by identifying the challenges they need to solve, then determine which AI solutions can help.

An impressive model and a valuable manufacturing application are not the same thing. Identify where there are downtime, quality losses, maintenance demands, throughput constraints, or engineering bottlenecks creating measurable consequences. Then work backward from that problem to determine what data, workflows, and intelligence could change the result.

According to Chris Stevens, President of Siemens U.S. Digital Industries, successful deployments begin with the business problem and determining how the data, workflow, and user experience can produce a measurable outcome.

Predictive maintenance provides a useful example. BlueScope began deploying Siemens Senseye Predictive Maintenance to identify abnormalities before equipment failures occurred. Siemens reports that the initiative has avoided more than 1,950 hours of machine downtime across locations worldwide and prevented 53 complete process stops. That is a much more meaningful Industrial AI metric than the number of models deployed.

The lesson applies beyond maintenance. Quality, throughput, or engineering time can be equally strong starting points when they constrain performance. The common denominator is an operational baseline connected to a measurable outcome. Industrial AI earns the right to scale when the manufacturer can point not simply to what the technology produced, but to what changed in the operation because of it.

What changes when Industrial AI starts influencing operations?

The risk equation changes when AI moves from providing information to influencing engineering, maintenance, or production decisions.

A recommendation in an office workflow may be reviewed, modified, or discarded without affecting a physical process. A recommendation that changes a machine parameter, control sequence, or maintenance action can have operational consequences. The closer AI gets to physical execution, the more important context, validation, permissions, and human oversight become.

We already see this boundary moving. IMA Group is working with Siemens to introduce Industrial AI into packaging-machine control. Production scenarios are simulated in a digital twin to generate synthetic training data before a neural network is embedded in a PLC for real-time motion control and adaptive machine behavior. The approach allows models to be trained and validated before physical commissioning.

NIST is examining the same emerging challenge from the standards perspective. Its 2026 manufacturing workshop focused on development and validation of AI-driven operations, maintenance, and control strategies, along with trust, safety, and evaluation of AI's effects on physical processes and assets.

So greater AI capability should not mean weaker controls. It should mean a more deliberate path from insight to recommendation to validated action. The more consequential the decision, the stronger that path needs to become.

How can Industrial AI work in brownfield manufacturing?

Integrating Industrial AI into existing factories brings particular challenges: equipment, automation systems and sensors vary in age and capability, and available data may not have been collected with AI in mind.

That makes interoperability and deployment architecture as important as model performance.

BlueScope's global predictive-maintenance rollout illustrates the practical reality. The program encountered legacy equipment, outdated sensors, and limited infrastructure, as well as data originating in systems including HMIs and PLCs with different update rates and formats. Rather than waiting for perfect data, teams assessed available information and supplemented it where necessary. As BlueScope standardized what it learned, the Western Port operation progressed from setup to its first predictive-maintenance success in three months, versus 18 months for the initial pilot.

Audi demonstrates another dimension of the challenge. Working with Siemens, the automaker uses Industrial Edge infrastructure that supports virtual PLCs and AI solutions. Its AI models identify defects including cracks and weld splatters, while the standardized infrastructure provides a way to integrate AI into the automation environment and deploy it more broadly.

For U.S. manufacturers, the implication is important. Industrial AI does not require every existing asset to become new. Scaling depends instead on connecting available data and automation in a repeatable architecture that can accommodate the heterogeneity already on the factory floor.

For U.S. manufacturers, AI creates value when it solves a measurable operational problem, works inside mixed technology environments, and earns enough trust to influence physical operations. Operations must perform better because of it.

Why does domain expertise matter more as Industrial AI becomes more capable?

General AI can recognize patterns in tremendous volumes of information. Industrial AI must understand what those patterns mean inside a physical process.

That is where domain expertise becomes more, not less, important.

Industrial data carries context: a temperature change may be normal under one operating condition and a warning under another. A maintenance recommendation has to account for the asset, operating history, and production environment. An engineering change must respect physical constraints. Siemens' emphasizes the same requirement: organizations need contextualized data and workflows that put AI insights in the right hands at the right moment rather than requiring engineers to navigate disconnected AI tools.

And expertise itself is under pressure. The U.S. Bureau of Labor Statistics projects nearly 1 million openings in production occupations each year, on average, from 2024 through 2034, largely because workers leave occupations permanently, including through retirement or occupational transfers.

Industrial AI therefore has an important role not simply as an automation layer, but as a mechanism for making existing knowledge more accessible.

At the Siemens Electronics Factory Erlangen, for example, a generative AI assistant helps employees troubleshoot machinery using industrial information. Interviews with maintenance engineers indicate an average 25-percent savings in reactive-maintenance time.

The objective is not to separate AI from human expertise. It is to combine AI's scale with the context and judgment that make industrial knowledge useful.

How can digital twins validate Industrial AI before deployment?

If Industrial AI is going to influence a physical system, manufacturers need a place where recommendations can fail safely.

A digital twin can provide that environment.

The principle is straightforward. Instead of moving directly from an AI-generated recommendation to a live production change, manufacturers can evaluate the proposed change virtually. A digital twin can test multiple scenarios and confirm expected outcomes before physical implementation. As AI moves from identifying problems toward recommending actions, that validation becomes increasingly important.

IMA Group offers a concrete example. The company uses production scenarios simulated in a digital twin to generate synthetic data for training control models. This reduces physical testing and enables validation before commissioning; the trained neural network can then run in the PLC to support adaptive machine behavior.

The larger point is that simulation becomes strategically more valuable as AI becomes more operational.

A model's confidence score alone cannot tell a manufacturer whether a proposed decision will behave correctly within the constraints of a real machine or process. A digital twin can create a bridge between computational intelligence and physical reality by allowing potential outcomes to be assessed before production bears the risk.

Trust, in that sense, does not have to mean taking the AI's word for it. It can come from testing the recommendation.

When do Industrial AI copilots and agents create real value?

Copilots create their greatest value when they reduce the distance between a worker's problem and the expertise needed to resolve it.

That can mean locating complex technical information, interpreting error information, assisting troubleshooting, or supporting engineering workflows. At Erlangen, the Industrial Copilot approach gives production employees access to an AI-powered assistant on the shop floor. Siemens reports that maintenance-engineer interviews indicate about 25-percent less reactive-maintenance time. Importantly, the employee still determines whether recommendations involving machine settings or other solutions are appropriate.

Agents raise the stakes further because their emerging role is not merely answering questions but reasoning, planning and potentially acting across manufacturing workflows. NIST describes agentic AI as a critical frontier for engineering and operations while noting that wide-scale adoption is constrained by concerns about reliability, safety and the absence of standardized performance metrics. Its work specifically highlights the need to validate agentic decisions.

That suggests a sensible dividing line. Manufacturers can move more quickly where AI retrieves knowledge, synthesizes context and supports human decisions. They should demand progressively stronger validation and governance as AI moves toward actions affecting physical operations.

Autonomy should therefore be viewed as a progression, not a switch: assist, recommend, validate, and only then automate where the operational evidence justifies it.

How should manufacturers measure Industrial AI success?

The number of pilots, models, copilots, or agents deployed tells us very little about whether a factory is getting better.

The metrics that matter already exist inside manufacturing: downtime avoided, scrap reduced, throughput increased, maintenance time shortened, commissioning accelerated, quality improved, and engineering hours returned to people.

That distinction is particularly important because AI adoption can run ahead of operational integration. In the Dallas Fed's May 2026 Texas Business Outlook Surveys, two-thirds of overall responding firms reported using AI, yet the Fed said use was largely occurring in testing or piloting or among a small share of employees. Among the relatively limited group of 43 responding firms where AI was used regularly by many employees, 62.8 percent said AI was integrated into core business processes and/or operations.

For manufacturing specifically, that journey from experimentation to operational value should be judged on outcomes.

BlueScope's more than 1,950 hours of avoided downtime and 53 prevented process stops provides one model. Erlangen's reported 25% average reduction in reactive-maintenance time provides another. These numbers measure the operation, not the novelty of the technology.

That is the standard Industrial AI now has to meet.

The next phase of AI in manufacturing will not be defined by asking how much AI a manufacturer has deployed. It will be defined by a harder and ultimately more valuable question:

Is the operation measurably better because AI is part of it?

Published: October 27, 2026