SCAMM aimed to modernize its systems by adopting advanced automation standards. The challenge was managing long and complex production lines while improving usability and reducing engineering times. Together with Siemens, the company implemented a solution based on WinCC Unified as the new HMI standard, optimizing Motion Control for cutting-edge results.
Technological excellence in sheet metal processing
Digital solutions for sheet metal forming

Centralize complex line management
Thanks to WinCC Unified and Collaboration technology, the operator interface is managed from a central PC, simplifying supervision and improving usability.

Increase performance and reduce cycle times
Integrating PLC, advanced Motion Control, and Safety functions in a single environmente allows managing complex operations with one flexible system.

Reduce engineering and commissioning times
Using a single development environment and a standardized HMI platform simplifies future upgrades, ensuring scalability and long-term efficiency.
SCAMM in action: flexibility and control
Gain complete visibility for fast decisions
Adopting WinCC Unified allowed SCAMM to create a modern, user-friendly interface. The system is fully adaptive: the HMI dynamically configures itself based on PLC data, while alarms are defined directly in the PLC using ProDiag. This architecture ensures operators always have critical information at hand, simplifying the supervision of complex processes and reducing the risk of operational errors.


Maximize performance with integrated systems
The integrated Siemens solution allows SCAMM to manage sophisticated machinery with a single, powerful system. Combining the reliability of SIMATIC S7-1500 with the power of an industrial PC, SCAMM achieves reduced cycle times and high performance. Collaboration technology enables a smooth flow of information between stations, turning technical complexity into a competitive advantage.
Ensure scalability and value over time
Ensure scalability and valLa standardizzazione della piattaforma HMI e l'uso di un ambiente di sviluppo unico assicurano una coerenza operativa senza precedenti. Eventuali aggiornamenti futuri delle macchine richiedono modifiche solo a livello di PLC, poiché l'interfaccia si adatta dinamicamente ai nuovi parametri. Questo approccio protegge l'investimento del cliente, garantendo efficienza a lungo termine e la capacità di rispondere rapidamente alle nuove richieste di un mercato in continua evoluzione.ue over time

With this project, we have chosen to redefine the future of our machines. A future that Siemens, as a Tech Company, is actively shaping — seamlessly integrating automation, software, and motion control to transform technology into measurable business value.