Skip to main content
Company Core Technologies

Computing and Communication

Our research covers software and communication infrastructure for Siemens products from the field to the cloud. It includes operating systems, runtime, middleware, networking, app management, data processing and emerging computing technologies.

What if we could seamlessly connect real and digital assets from the field to the cloud?

The key lies in advanced industrial edge platforms and unified communication architectures. By bridging physical machines directly to digital and software ecosystems, these systems enable instant data exchange, rapid deployment of software updates and precise automated control across the modern shop floor.

What matters are industrial edge platforms and communication architectures that seamlessly connect physical assets with digital environments.

Split image showing a glowing microchip processor and two engineers connecting cables to hardware devices.
Automated manufacturing facility with autonomous mobile robots connected via cyan light network graphics and a 5G logo.

Computing & Communication technologies cover industrial communication, deterministic wireless, telco standards and intent-based networking across 5G/6G, Non-Terrestrial, WiFi, wired and TSN. They include device connectivity, zero-touch onboarding and field-to-cloud interoperability via middleware like OPC UA, DDS, and MQTT.

This domain spans software stacks for virtualization, container orchestration, edge management and OT-grade operating systems ensuring real-time determinism and safety. Additionally, it addresses platform observability, resilience mechanisms, AI enablement across compute fabrics and emerging computing paradigms like quantum computing.

This Company Core Technology comprises applications and systems cover software stacks and standardization for general-purpose, application-specific, and real-time computing across field and edge devices. They enable software-defined automation and control across single-node to full-plant setups, managing mixed criticality, real-time execution and resilient orchestration.

Computing & Communication comprises the field-edge-cloud continuum with open standards, industrial operating systems, device onboarding and interoperable data exchange. Additionally, it encompasses lifecycle observability, edge data processing and operational support across industrial infrastructures.

Icon for Computing & Communication
Publications

Explore our featured papers


Data centers manufacturing steel: rethinking industrial networks in the age of IT

Published in: HotNets '25: Proceedings of the 24th ACM Workshop on Hot Topics in Networks, pages 85 ‑ 95
Nikolaos Mitsakis, Marco Reisacher, Matthias Eichholz, Yannic Breiting, Harald Albrecht, Andreas Blenk, Oliver Hohlfeld

Industrial networks are undergoing a shift from static OT environments to open networks integrating IT and OT. This transition applies IT operational principles to OT, such as virtualizing Programmable Logic Controllers and leveraging AI to boost efficiency. However, this paper shows that IT/OT convergence remains an underexplored research area, missing key opportunities for future networking systems. We highlight three core challenges: timing constraints, service availability and changing traffic dynamics. For each, we present a use case detailing preliminary findings and defining new research avenues for SIGCOMM.
View at publisher's page


LLMs on edge: Network traffic characteristics of distributed inference under the loupe

Submitted to: NAIC '25: Proceedings of the 2nd Workshop on Networks for AI Computing, pages 108 ‑ 114
Philippe Buschmann, Arne Broering, Georg Carle, Andreas Blenk

Large language models (LLMs) are expanding from cloud deployments to edge computing environments, including end-customer devices and industrial settings. However, deploying LLMs at the edge presents unique challenges due to network infrastructure and resource limitations. Although distributed LLM frameworks have emerged to optimize edge deployments, they are still in the early stages of development and have not undergone comprehensive real-world testing. This paper evaluates the performance of distributed LLM frameworks in edge environments, revealing unexpected drops in performance when adding compute nodes and uncovering complex network traffic patterns.
View at publisher's page


Interoperable cyber-physical multi-agent systems through Web of Things

Published in: 2025 International Conference on Web Engineering
Roman Binkert, Fady Salama, Ege Korkan, Sebastian Käbisch, Sebastian Steinhorst

The rise of IoT systems has introduced multi-agent systems (MAS) as a means of managing growing complexity via autonomous, self-organizing agents. However, existing MAS frameworks suffer from fragmentation, limited agent interoperability and complex cyber-physical system (CPS) integration. To address these issues, we introduce the Web of multi-agent things (WoMAT), which incorporates the W3C Web of Things (WoT) standard directly into agent communication. By mapping WoT interaction affordances to AgentSpeak performatives, WoMAT enables seamless, protocol-independent interaction and semantic interoperability using ontology-enriched thing descriptions. Implemented with the JaCoMo framework, WoMAT establishes MASs as a viable edge solution.
View at publisher's page


A survey on satellite computing: Connecting the dots between networks and applications

Published in: 2025 IEEE Communications Surveys & Tutorials (Volume: 28)
Carlos Guimarães, Alessio Netti, Markus Sauer, Florian Zeiger, Hans-Peter Huth, Elizaveta Boriskova

Rapid advancements in satellite technology, driven by low Earth orbit (LEO) mega-constellations and inter-satellite links, have rekindled interest in satellite computing as a means of providing edge computing services worldwide. Despite growing research in this area, the field remains fragmented and unstandardized, and its role in beyond-5G/6G systems is unclear. This survey addresses these gaps by evaluating the networking and computing factors that impact satellite computing, as well as its key applications. The paper presents a taxonomy based on application requirements and design choices, offering an industrial perspective and outlining open challenges to guide future research.
View at publisher's page


Open-source SBOM generator for Debian-based distributions

Published in: 2026
F. Mößbauer, C. Steiger, T. Larisch, M. Adler, G. Hillier

debsbom generates software bills of materials (SBOMs) for Debian-based distributions in SPDX and CycloneDX formats. SBOMs list both installed binary packages and Debian source packages. This is crucial for security tracking because Debian CVEs are assigned to source packages rather than binary components. Additionally, debsbom creates a complete dependency graph of the analyzed system. This allows users to identify critical distribution components and determine which package dependencies introduced specific vulnerabilities.
View at publisher's page