Skip to main content
INFRASTRUCTURE

Building efficiency starts with existing buildings

By: Eric Harting, Portfolio Manager, Building Technology

For building owners and operators, improving performance does not always have to begin with a major capital project. In many existing U.S. buildings, the first opportunity is to get more from assets already in place: understanding where energy is being wasted, identifying systems that are underperforming and using better controls to operate equipment more efficiently. That opportunity is increasingly important as electricity demand grows and owners weigh competing demands for capital. U.S. electricity demand has increased an average of 2.1 percent annually over the past five years, according to the U.S. Energy Information Administration, which projects continued growth through 2050.

That changes the economics of building energy efficiency. Instead of viewing efficiency primarily as a sustainability initiative or waiting for the next major equipment-replacement cycle, owners can look at the physical operation of the building itself. Where is energy being consumed unnecessarily? Which assets are operating outside expected ranges? Which adjustments can be made now, and which equipment problems truly require capital?

For U.S. building owners and operators, the fastest path to lower energy cost and emissions often starts with the buildings they already have. The business case is operational: use better data and controls to reduce waste, improve equipment performance, and prioritize capital without waiting for a full retrofit or replacement cycle.

Building energy efficiency creates four value pools

The business case for building energy efficiency becomes clearer when we separate its potential sources of value rather than treating every benefit as interchangeable.

The first and most direct is the cost of energy consumption. Reducing unnecessary heating, cooling, ventilation, and other loads can lower consumption and operating expense. That is a hard-dollar benefit when it is measured against an appropriate baseline.

The second is maintenance and asset life. Building data can help operators see abnormal equipment behavior and target maintenance where it is needed. The financial effect will depend on the building and equipment involved, so it should be evaluated independently from energy savings rather than assumed.

The third is operational resilience. Better visibility into how building systems are performing can help operating teams recognize problems earlier and make more informed decisions about critical assets. As energy demand grows and grid conditions become more important to business planning, knowing how, when and where a building consumes energy becomes an operational capability, not simply a sustainability metric.

The fourth is occupant conditions. Temperature, humidity, air quality, and consistent environmental conditions matter in workplaces, schools, and other occupied spaces. But the economic benefits should not be overstated. Better indoor conditions may support an owner's broader objectives, but claims about productivity, occupancy, lease rates, or profitability require evidence specific to the building and use case. Modifying building operations shouldn't occur at the expense of occupant comfort.

Separating these four value pools matters. It allows an owner to distinguish measurable savings from other valuable but more context-dependent operating benefits.

Existing building optimization avoids starting over

This is where the economics of America's existing building stock become especially important.

Owners rarely have the luxury of treating a building as a blank sheet of paper. Buildings may contain HVAC equipment installed at different times, multiple generations of controls, components from different manufacturers, and systems that still have useful operating life. Even when a major modernization is justified, replacing everything at once may be neither financially sound nor operationally feasible.

That makes existing building optimization largely an interoperability problem: How do we obtain useful information from the systems already there and turn it into better operating decisions?

The answer should not automatically be rip and replace.

Open, interoperable digital building systems can create a layer across existing infrastructure, allowing owners to connect operational data and improve visibility while preserving usable assets. Siemens' Building X, for example, is designed as a central foundation for collecting and analyzing real-time building data and provides open APIs for integrating building systems across multiple vendors. Siemens says customers using the platform have achieved energy savings of up to 30 percent through data-driven energy-efficiency optimization. That figure, however, is a reported customer outcome, not a guaranteed result for every building.

The larger point is more important than any individual platform: digitization creates the most value when it helps owners improve the economics of assets they already own rather than forcing technology modernization and physical replacement to happen at the same time.

Better building energy management turns data into action

Data alone does not save energy.

Its value comes from the operational chain it enables: visibility, diagnosis, control, and verification.

First, owners need visibility into what a building and its major systems are actually doing. Energy and operating data can reveal when and where consumption occurs and establish the baseline against which changes can be measured.

From there comes diagnosis. Operators can investigate high-load or high-variance systems and look for operating patterns that indicate waste or malfunction: equipment running when it is not needed, conflicting heating and cooling, excess ventilation or control settings that no longer correspond to occupancy and use.

Then comes control. Once causes are understood, operators can adjust schedules, setpoints and sequences or address equipment that is not functioning as intended.

Finally comes verification. Did the intervention actually reduce consumption or cost relative to the baseline? If not, why not?

That last step is critical because it turns building energy management from a collection of activities into a repeatable business process. Owners can distinguish changes that produce measurable results from those that do not, and they can use that evidence to decide where the next dollar of capital or operating budget should go.

For U.S. building owners and operators, the fastest path to lower energy cost and emissions often starts with the buildings they already have. The business case is operational: use better data and controls to reduce waste, improve equipment performance, and prioritize capital without waiting for a full retrofit or replacement cycle.

How to prioritize existing building improvements

A practical approach does not begin with a technology shopping list. It begins with a sequence of operating questions.

1. Establish the baseline Understand current energy consumption, operating schedules, and major loads. Without a credible starting point, savings are difficult to verify.

2. Identify high-load and high-variance systems Focus attention where consumption is greatest or performance deviates significantly from expected patterns. HVAC is often an important area to investigate because heating, cooling, and ventilation are controllable building loads.

3. Optimize existing controls Before replacing functioning assets, determine whether schedules, setpoints, ventilation levels, and sequences can be better aligned with actual building use.

4. Fix the biggest equipment problems Data and operational analysis can help separate inefficient operation from equipment that genuinely needs repair, modernization, or replacement.

5. Verify the result Compare performance against the baseline and establish whether the improvement produced the intended savings.

This sequence also creates a more disciplined way to allocate capital. Some opportunities may be primarily operational. Others will require equipment investment. The point is to identify which is which before treating wholesale replacement as the default answer.

Financing can also be part of that calculation when larger improvements are justified. Siemens reports that it has delivered more than 1,000 performance contracts producing $2 billion in operational and energy savings. Energy savings performance contracts can use savings generated by projects to help fund infrastructure improvements.

Existing buildings can deliver measurable energy savings

There is already evidence of what this approach can look like when existing infrastructure becomes the starting point.

AI-enabled optimization provides one example. Oxoia connects to existing Siemens building automation and analyzes information from HVAC systems, sensors, occupancy, indoor climate and weather. It can recommend adjustments or automatically optimize HVAC operation based on those inputs. Siemens says the technology has been deployed in more than 100 buildings and has delivered verified energy savings of up to 35 percent, with a typical payback period of 12 months and no hardware replacement required. Operations do not have to be interrupted during installation.

Those figures should not be interpreted as a universal savings forecast. Building type, existing performance, equipment, climate, occupancy and operating practices all influence the opportunity. But the example demonstrates the underlying principle: measurable improvements can sometimes come from changing how existing physical systems operate before replacing those systems.

This is also where AI building optimization becomes useful, but only after the fundamentals are in place.

AI can analyze operating patterns that are difficult to follow manually and continually adjust HVAC operation as variables such as occupancy, indoor conditions and weather change. Oxoia, for instance, analyzes building data continuously and can automatically adjust HVAC settings while allowing facility managers to retain visibility and intervene.

The sequence matters. AI is not a substitute for usable building data, functioning controls or sound operating practices. Its value increases when systems can reliably provide the information needed to detect inefficiency and act on it.

Building efficiency is the bridge to better operations

The strongest business case for improving an existing building may be simpler than we sometimes make it.

Start with energy being paid for today. Understand how existing assets are performing. Correct avoidable waste. Identify equipment that genuinely requires investment. Verify the savings. Then use what the building tells you to determine the next improvement.

That approach connects sustainability to something owners already understand: operational performance.

It also changes the role of technology. Rather than beginning with the question, What new system should we install? existing building optimization begins with a more useful question: What can we improve in this building without starting over?

At Siemens, that is increasingly how we see the opportunity. Digital platforms such as Building X can provide centralized, real-time building data and support energy, operations, and maintenance use cases, while AI-based optimization can extend that foundation toward increasingly continuous and automated operation. But technology is the enabler, not the economic argument.

The argument is the building itself.

For owners navigating growing energy demand, aging systems and limited capital, efficiency can become the bridge between the infrastructure they have today and the higher-performing building they need tomorrow. Lower energy consumption can reduce operating cost. Better information can sharpen maintenance and capital decisions. More responsive controls can strengthen day-to-day operations. And every verified improvement gives the owner stronger evidence for deciding what to do next.

The fastest way forward may not be to start over. It may be to make the building you already have work better.

Published: November 9, 2026