Skip to main content
e455ab74-16b2-40aa-93ff-44b902ccde9d - aral-pulse-key-visual-digital-twin-shero-2560x1440
Case study

Get the unseen right and help electromobility take off

At Aral pulse, high-power charging is front and center. Behind the scenes, Siemens tech and engineering unite real infrastructure with digital smarts, ensuring every charge is fast, seamless, and reliable. Powering Germany’s shift to electric mobility and the energy transition.

Webinar: How to manage increased truck charging demand

Learn how DSOs can support electrifying the transportation sector without increasing CapEx and OpEx

An intelligent charging network throughout Germany with Electrification X

Growth, security, and future go without saying: Scaling a fast charging network like Aral pulse is anything but simple. But with Electrification X, up to 600 smart local grid stations run centrally managed, securely, and without friction.

Flooded by vulnerability notifications? NIS2 compliance issues? Escalating cyber threats? Complex patch management workflows? You won’t see any of it because it’s already handled. That’s how we keep this network growing.

4ce90e18-1f71-47fb-8c2e-7e8809692fce - aral-pulse-electrification-x-illustration-no-text-mhero-1280x720

Electrification X provides:

  • Increased uptime via remote control
  • Optimized OPEX via real-time monitoring
  • Dynamic load management of ultra-fast charging stations (up to 400 kW capacity)

NIS 2 compliance:

  • NIS 2 conditions for critical infrastructure
  • Network operator requirements according to VDE4110
At Aral pulse, our goal is to make ultra-fast charging as effortless and available as traditional refueling. To accomplish this, we are partnering with Siemens and investing in more than 650 stations across Germany – a digital, future-ready charging infrastructure.
Alexander Junge, Member of the Executive Board of Aral AG and, General Manager bp pulse Central Europe

Highlight figures

600 intelligent local grid stations

Up to 600 intelligent local grid stations centrally managed

400kW charging power

Up to 400 kW charging power each for cars

350 km charging speed

Up to 350 km reach in 10 minutes

1K kW charging power

Up to 1,000 kW charging power each for trucks

Powering the future of EV charging at Aral pulse

Explore the Aral Pulse Gigahub in Mönchengladbach – the first of its kind with 28 ultra-fast chargers. Siemens’ Electrification X enables efficient load management, near real-time monitoring, and secure remote servicing, boosting transparency, cutting costs, and supporting Germany’s EV future.

Power, intelligence and performance that counts

Intelligent substations and Electrification X create a perfectly synchronized hardware-software foundation for fast-charging at scale. It connects real-world power infrastructure with digital intelligence, making it reliable, secure, flexible, and ready for whatever comes next.

Transforming power. And the everyday.

Though the intelligent substation may stand quietly at the edge of the site, its crucial medium-voltage link makes fast charging possible. With its sealed transformer, 8DJH gas-insulated switchgear, and SIVACON S8 low-voltage board for up to six high-power chargers, it connects each station seamlessly to the public grid. All its components are communication capable to enable remote monitoring and near real-time load management that ensure the energy flows exactly where it’s needed – day in, day out.

Unseen, but always in charge

Electrification X keeps every charger and substation connected, monitored, and optimized in near real time, from one central platform. Dynamic load management ensures efficient power use, while remote control and security features keep the entire network stable, protected, and ready to scale. And because diagnostic data is consolidated in one place, issues are resolved faster – maximizing uptime across every site.

For everything today. And anything to come

Electrification X is built to evolve, not just to operate. Its open, vendor-neutral architecture keeps the charging network flexible as new requirements emerge: From integrating renewables to connecting with grid operators or adding new applications at scale. Because all assets are cloud-enabled and centrally managed, the deployment of upgrades and new functionalities won’t disrupt operations. The result: a fast-charging infrastructure that grows with demand, adapts to new technologies, and stays future-proof as mobility continues to change.

With Electrification X, we’ve gained full transparency across our fast-charging network. Today, more than 300 local substations are digitally connected and monitored, with the added benefit of being able to resolve many issues remotely.
Alexander Junge, Member of the Executive Board of Aral AG and, General Manager bp pulse Central Europe

Contact us

For more information on Electrification X, contact our experts.