Skip to main content
A visual representation of a battery storage system for renewable energy transition with a focus on lithium-ion technology.

Stoccaggio delle batterie: Attore chiave nella transizione energetica rinnovabile

Finanziare progetti di stoccaggio di batterie offre un percorso verso la decarbonizzazione

JUNE 2023

Battery storage systems have become an essential component of renewable energy infrastructure as the world seeks to transition away from fossil fuels. It helps to ensure a reliable and consistent supply of electricity, especially in areas where renewable energy sources like wind and solar are prevalent. Many states are turning to clean energy as a critical step to decarbonizing the transportation and power sectors, which are responsible for 55% of greenhouse gas emissions in the United States.

Siemens Financial Services (SFS) is at the forefront of financing battery storage projects, having financed 2,100 MW / 5,411 MWh of standalone battery storage in the Americas in recent years, along with additional capacity as part of solar plus storage projects. Most recently, SFS helped various customers including EnerSmart, Javits Center, Clearway Energy Group, and others achieve their goals.

EnerSmart is developing intelligent energy storage systems that use predictive analytics and big data to make the electric grid more reliable. The San Diego-based company required financing to provide critical battery infrastructure for energy storage in the San Diego area. SFS and the North American Development Bank (NADBank) provided a $78.2 million loan facility to finance the development and operation of EnerSmart's utility-scale energy storage projects. The portfolio will be capable of storing up to 330 MWh of electricity, the equivalent of supplying 110,000 customers for up to two hours. The projects will help integrate electricity generated by intermittent renewable energy sources such as wind and solar, displacing carbon emissions.

Siamo entusiasti di collaborare con Siemens e NADBank su questo finanziamento innovativo del progetto che aiuterà a consentire la continua crescita ed espansione dell'energia rinnovabile senza carbonio per le comunità di San Diego.
Marc La Magna, Co-CEO, EnerSmart

Clearway is developing two utility-scale solar and storage projects in Riverside County, California, on U.S. Bureau of Land Management land. The projects will have a combined capacity of 463 MW of clean energy capacity and 186 MW of battery storage, which is enough to power 132,000 homes annually. SFS is among a club of lenders that committed approximately $1 billion to the development of the two solar plus battery storage facilities.

Apprezziamo la fiducia e il supporto delle nostre banche partner per unirsi e formare una delle più grandi strutture di finanziamento per la costruzione nella storia di Clearway. La formazione di capitale per progetti di energia rinnovabile a questa scalabilità, e le capacità dei principali sviluppatori come Clearway di portare a termine tali progetti, saranno un fattore distintivo nel raggiungimento degli obiettivi della transizione energetica negli Stati Uniti.
Steve Ryder, Direttore Finanziario, Clearway

In addition to EnerSmart and Clearway, Aypa Power is another company using battery storage systems to accelerate the adoption of renewable energy. As Lead Arrangers, SFS, along with CIT, a division of First Citizens Bank, has closed an $84.5 million project financing for Aypa Power’s Wolf Tank energy storage project in Texas. Wolf Tank is a 173 megawatt-hour standalone battery storage project that will begin commercial operations in 2023.

Lo stoccaggio di energia è un componente sempre più prezioso del mix di generazione elettrica, facilitando l'integrazione della produzione di energia rinnovabile nella rete elettrica e garantendo un flusso di elettricità affidabile. Abbiamo apprezzato il supporto, l'agilità e l'expertise di CIT e Siemens nell'organizzare il finanziamento per il progetto Wolf Tank.
Marc Atlas, Direttore Finanziario, Aypa Power

Plus Power combines data-driven algorithms with standalone energy storage to address grid congestion and wholesale market volatility. They announced completion of $1.8 billion in new financing and SFS served as Joint Lead Arranger for five new standalone battery energy storage projects totaling 1,040 MW of capacity across Texas and Arizona to help stabilize the U.S. electrical grid while incorporating solar and wind energy.

Similarly, SFS participated as a Joint Lead Arranger, along with BankUnited, N.A., in the financing of two Jupiter Power standalone battery energy storage projects in Texas totaling 160 MW.

Questo capitale supporterà l'attuale sviluppo del più grande e diversificato portafoglio di progetti di stoccaggio autonomi negli Stati Uniti. La scalabilità evidenzia il nostro vantaggio di primo arrivato nel portare progetti di alta qualità sul mercato, così come il lavoro straordinario del nostro fantastico team. Apprezziamo profondamente i nostri partner finanziari che supportano la costruzione e il funzionamento del nostro ampio portafoglio negli Stati Uniti, consentendo la decarbonizzazione e la transizione verso una rete più efficiente.
Josh Goldstein, Direttore Finanziario, Plus Power

Renewable energy integration by the C&I (commercial and industrial) and MUSH (municipalities, universities, schools, and hospitals) markets is hindered by the high up-front capital requirement associated with purchasing renewable energy infrastructure. To combat this, SFS committed $35 million to support Madison Energy Investments' portfolio of distributed solar and solar plus storage projects, representing over 200MW generating capacity in the U.S. primarily for these markets, using an Energy-as-a-Service (EaaS) model. The EaaS model gives customers access to environmentally friendly, reliable, on-site energy solutions with zero upfront capital required and predictable energy costs.

Riconosciamo l'importanza delle infrastrutture critiche nel plasmare il nostro futuro sostenibile. Con questo finanziamento del debito, siamo pronti a realizzare progetti innovativi e a svolgere un ruolo essenziale nella costruzione di un mondo più pulito e resiliente per le generazioni future.
Iwona Guier, Vicepresidente esecutivo delle finanze, Madison Energy Investments

Finally, the Javits Center is a great example of how battery storage can reduce energy costs and help meet aggressive solar and energy-storage targets. SFS provided debt financing to the Javits Center via its investment in Calibrant Energy*, helping them manage new energy technology through reduced costs in the form of lower $/kWh. The project includes nearly 2,500 solar panels and a 3.5-megawatt battery. The battery will allow excess generation from Manhattan's largest rooftop solar array to be stored for use during times of peak power demand, reducing energy costs and helping New York State meet its aggressive solar and energy-storage targets.

Il nostro tetto verde è diventato un modello di sostenibilità per gli edifici in tutto lo Stato di New York, e siamo orgogliosi di collaborare con la New York Power Authority per ampliare ulteriormente il nostro impatto ambientale. Da più di 30 anni, il Javits Center è un motore economico per New York, ma con questo progetto possiamo continuare a rafforzare la nostra reputazione come faro ambientale, fungendo da ispirazione per altre sedi in tutto il Paese.
Alan Steel, Presidente e CEO, New York Convention Center Operating Corporation

Energy storage complements intermittent variable energy resources by absorbing excess clean renewable energy and releasing that stored energy when needed to support and sustain grid reliability. SFS is proud to finance battery storage systems for renewable energy infrastructure projects, contributing to a more sustainable world and helping to pave the way to a net-zero future.

*As of August 2024, Siemens Industry, Inc. and Siemens Financial Services, Inc. no longer maintain an ownership interest in Calibrant Energy. All parties, however, continue to collaborate, seek, and provide solutions to facilitate the energy transition.

Inizia il tuo viaggio