Skip to main content

Catalyst for steel transformation

Digital transformation is supporting Tata Steel Nederland’s efforts to improve operational efficiency and reduce the environmental impact.

Tata Steel Nederland

Photo by Fix Media (fixmedia.nl)

By becoming a Digital Enterprise, Tata Steel Nederland is optimizing processes, ensuring high operational availability and supporting its transition toward cleaner production.

The steel industry is nearing a positive tipping point. Manufacturers across the globe are taking bold steps to cut the carbon footprint of one of the world’s most emissions-intensive materials. Europe sees the decarbonization of steel as strategic to its economic security and greater competitive edge.

Tata Steel Nederland is forging ahead with its own ambitious plans to reduce CO₂ emissions by 35-40% at its IJmuiden plant, one of the most CO₂-efficient conventional steel plants in Europe. Digital transformation is supporting Tata Steel Nederland’s efforts to improve operational efficiency and advance its sustainability objectives.

The data imperative

In the highly complex steel production environment, where continuity and security are essential, a Managed IT/OT Infrastructure is key. At the heart of Tata Steel Nederland’s Hot Strip Mill and Hot Dip Galvanizing Line in IJmuiden is our Industrial Automation DataCenter. This on-premises IT infrastructure is specifically designed for industrial environments. It centralizes production applications like SIMATIC PCS 7 on a platform that combines computing based on virtualization, data archiving, backup and restore capabilities as well as an IEC 62443-compliant network architecture for secure IT/OT data exchange. Tata Steel Nederland can rely on the infrastructure’s high availability, efficiency and cybersecurity.

However, such an IT/OT infrastructure requires ongoing maintenance including handling regular patching, ensuring the integrity of data backups, implementing updates and managing vulnerabilities. This is why Tata Steel Nederland also relies on our managed services Availability Care - Operate (formerly Remote Industrial Operations Services) to efficiently maintain the health and security of the Industrial Automation DataCenter. A team of experts continuously monitors and manages the IT/OT systems, detecting potential issues and resolving them swiftly before they have an impact on the operations. During initial implementation 25% of updates and backups were successfully fixed and since its deployment multiple system shutdowns have been prevented through continuous proactive monitoring.

Tata Steel IJmuiden - storage facility

Photo by Fix Media (fixmedia.nl)

From data to impact: Contributing to cleaner production with AI-based predictive maintenance

Effective maintenance is a key contributor to sustainability. Tata Steel Nederland took its Cold Mill Annealing Bay in IJmuiden to the next level of digitalization by implementing our AI-based Senseye Predictive Maintenance solution. Senseye uses shop floor data and AI-driven algorithms to predict and notify maintenance teams of potential problems, reducing the need for manual inspections. Its built-in generative AI CoPilot also empowers their maintenance teams by filling in knowledge gaps.

In the exhaust air cleaning unit, Senseye detected a mismatch between increasing fan speed and reduced airflow, indicating a clogged filter. The maintenance team replaced the filter and updated the control parameters, preventing harmful fumes from being released into the environment.

After installation, the number of machine breakdowns at the Cold Mill decreased by 67%, from 18 to six. Tata Steel Nederland enjoyed a return on investment within six months.

Steel still is the foundation of the modern world.

The global steel industry alone is set to account for nearly 35% of fossil fuel-related emissions by 2050. The time is now right for all industries to rethink business models, business priorities, and business sustainability
Sanjiv Paul, Vice President of Safety, Health & Sustainability, Tata Steel

Our collaboration with Tata Steel Nederland is helping shape scalable, secure and future-ready industrial operations and supports their transition toward cleaner production.