Skip to main content

AI-powered engineering

Redefine the bounds of engineering. From concept to operations, AI gives engineers the intelligence to design with greater confidence, manufacture with greater agility and optimize with greater speed across the full value chain.

Overview

What is AI-powered engineering?

AI-powered engineering is the application of artificial intelligence across the entire engineering lifecycle. At its core, it is built on machine learning and encompasses multiple forms of artificial intelligence — predictive, generative, agentic and more. It reasons across real-world operational data and simulation data, extracting patterns too complex for humans to see, revealing insights that empower engineers to make smarter decisions, drive automation and achieve continuous optimization.

Applications span areas such as:

  • AI-assisted design exploration
  • Generative design and optimization
  • AI-enabled simulation and validation
  • Requirements analysis and traceability
  • Engineering workflow automation

In practice, this means engineering teams can identify issues before they become costly, act on them with confidence and navigate the full complexity of the value chain rather than react to it.

Female engineer using AI technology for product development.
Challenges

Why engineering teams are turning to AI

Modern product development has never demanded more. Products now span structures, fluids, thermal systems, electromagnetics, electronics, controls and embedded systems, often all at once. They are increasingly software-defined, with more functionality, configurability and value living in code than ever before. And they have to be designed faster, with tighter compliance requirements, stricter sustainability targets and less tolerance for costly late-stage rework or physical prototyping.

The sheer number of disciplines involved, and the interactions between them, has outpaced what traditional engineering approaches can manage alone. Teams are expected to:

  • Move faster while managing more variables
  • Make better decisions earlier
  • Deliver more robust, compliant and manufacturable products from the start

That is exactly what AI-powered engineering makes possible.

Product engineer at computer using ai-driven processes to speed up product development

How AI-powered engineering supports product lifecycle

Building a great product is a journey of decisions, tradeoffs and iterations that spans years. AI-powered engineering puts intelligence to work at every stage of that journey, helping teams move faster, make better decisions and build products that perform in the real world.

Team of engineers discussing product requirements prior to design.

Concept and requirements

Before a single design is drawn, AI helps teams define what they're building and why. By connecting requirements to downstream engineering data, AI ensures that goals around performance, cost, sustainability and manufacturability are understood from day one, reducing costly misalignment later.

Female engineer using AI-powered design software to explore new product design possibilities.

Design exploration

Instead of evaluating a handful of options, AI enables engineers to explore thousands of design possibilities simultaneously. Generative design tools surface viable design alternatives that would otherwise go undiscovered, while AI-powered guidance helps teams understand how design parameters affect performance, weight, reliability and producibility, all before committing to a direction.

Team of engineers using ai engineering simulations to solve multiphysics challenges.

Simulation and analysis

Explore designs 1,000x faster than physics-based simulation with embedded AI. Physics predictions that once took days can now run in minutes using AI models trained on past simulation data. AI-trained simulation models make complex 3D design simulations practical at the system level, enabling digital twin deployment, multidisciplinary analysis and real-time performance evaluation without the computational overhead.

Simulation specialists at computer verifying and validating a new product design.

Verification and validation

AI streamlines testing by automatically identifying critical test scenarios, potential failure modes and risk areas so teams spend less time searching for problems and more time solving them. By continuously syncing the digital twin with real-world data, AI creates a closed-loop connection that allows teams to de-risk physical testing before a single prototype is built. Design errors are flagged early by comparing outputs against accepted standards, preventing flawed products from making it downstream.

Factory manager using AI predictive maintenance systems to monitor shop floor.

Manufacturing and production

AI bridges the gap between design intent and production reality. By incorporating manufacturing constraints and material behaviors directly into simulation-driven design, teams can evaluate production feasibility early and avoid late-stage surprises on the factory floor. From there, AI enables adaptive manufacturing through smart production planning and scheduling, allowing production lines to respond dynamically to changes in demand or operational conditions. Quality inspection is transformed through AI-driven computer vision and anomaly detection, ensuring consistent product standards at scale.

Factory manager using AI predictive maintenance systems to monitor shop floor.

In-service operation

Once a product is in the field, AI keeps working. Predictive maintenance systems process sensor data to detect patterns indicative of potential failures before they happen, reducing downtime and preventing costly breakdowns. Operational insights feed back into design and planning processes, creating a closed improvement loop where real-world performance continuously refines the entire development lifecycle.

Use cases

See AI-powered engineering in action

Across automotive, aerospace, electronics, energy, manufacturing, heavy equipment and life sciences, engineering teams are already using AI to solve their hardest challenges, and the numbers speak for themselves.

Explore 100 real-world use cases in one resource, showing exactly how AI-powered engineering is helping teams run faster simulations, cut analysis time and build more reliable products. Think 100x faster NVH analysis, a 600% boost in avionics reliability and 15x faster e-motor design, just to name a few.

Digital thread

One thread. Every decision.

Complexity compounds when teams, tools and data don’t speak the same language. Explore how a unified digital thread connects people, data and decisions across the entire development lifecycle.

How unified digital thread unifies through software defined products, multidomain collaboration, AI and simulation.

How to implement AI-powered engineering

AI adoption doesn't have to be overwhelming. From first steps to measuring success, this practical roadmap breaks down exactly how to modernize your engineering processes step by step.

Learn how to champion AI within your organization, navigate the complexities and unlock new possibilities in data-driven engineering. Real-world examples included.

Man at desk with two monitors, analyzing data on screens, with a blue background displaying numbers and a green line.
AI in product development

What makes AI-powered engineering possible

Predictive AI

Predictive AI analyzes historical and real-time data to identify patterns and forecast future outcomes, supporting human decisions vs. acting autonomously. Predictive maintenance systems are one of many engineering applications.

Generative AI

Generative AI goes beyond analysis to creation, producing designs, code and simulations from existing data. Where predictive AI forecasts what will happen, generative AI imagines what could be, helping teams innovate faster.

Physics-informed AI

Physics-informed AI embeds laws like gravity, thermodynamics and fluid dynamics into AI models as guardrails. This enables accurate predictions with limited data, helping teams model complex systems and accelerate development.

Physical and embodied AI

Physical AI lets machines sense and respond to the real world, powering robots and autonomous vehicles. Embodied AI, a subset, learns through physical interaction via sensors and actuators rather than pre-programmed responses.

Agentic AI

Agentic AI perceives, reasons and acts autonomously, accomplishing goals without step-by-step guidance. Unlike copilots, it executes tasks end-to-end. As a newer approach, responsible adoption is still being shaped.

FAQ

Related questions about AI-powered engineering

Learn more

Watch

On-demand webinar | Accelerating Innovation: AI for advanced multi-disciplinary design optimization

Read

Ebook | From complexity to competitive advantage: AI-powered performance engineering

White paper | Revolutionize product design with AI: The future is now with NX and Xpedition

Blog | AI in product development

Let's talk!

Reach out with questions or comments. We are here to help!