Skip to main content
This page is displayed using automated translation. View in US English instead?

Project PEARL

Optimal performance, occupant comfort, and energy efficiency are fundamental requirements for high-efficiency laboratories. Project PEARL (Performance for Efficient Airflow Regulation in Laboratories) is the world's first independent performance test designed specifically for lab environments.

Interdependent Data for high-performance laboratory environments

Project PEARL delivers objective insights and practical advantages to professionals responsible for creating superior, safer, and more sustainable laboratory environments globally. This independent approach enables evidence-based decision-making for ventilation optimization, energy management, and occupant safety improvements.

Project PEARL: Unbiased, comprehensive results for your lab facility

  • Three leading ventilation systems
  • Seven different configurations
  • Nine key performance factors

PEARL simulates realistic lab scenarios using heat loads, smart sensors, and remote-controlled systems to test three different laboratory ventilation setups under identical conditions. Through extensive trials in a strictly comparable and controlled environment, the project has delivered breakthrough findings that will reshape lab ventilation standards worldwide.

Setup in a lab for ventilation testing

Expert session: optimizing lab environments

Learn how modular lab approaches & airflow strategies set new safety, adaptability & research integrity standards.

The test subjects:

Three leading laboratory ventilation

We tested three different laboratory ventilation systems in our strictly comparable and controlled lab environment.

Select...

HL-X-VENT™ is an advanced ventilation solution designed for laboratory and industrial environments, forming a core component of the HL-X-LAB™ modular infrastructure system. It focuses on draft-free air semi-laminar airflow distribution, energy efficiency, and high safety standards for critical spaces and environments like BSL labs and cleanrooms.

air ventilation

Get personalized insights for your laboratory

Contact us to explore how PEARL´s performance data can optimize your ventilation system and improve efficiency.

The core evaluation factors: Key questions behind the laboratory ventilation experiment

Our comprehensive testing protocol examines critical performance metrics under real-world laboratory conditions, measuring everything from energy efficiency to air quality control to determine which system delivers superior results.

Select...

How effectively does the ventilation system maintain a stable and safe laboratory environment? We looked at areas like temperature stratification and air distribution, so the profile of temperatures and air velocities was recorded over the entire room.

Animated graphic for Airflow regulation

Video deep dive: How we built the world’s first real-life ventilation test zone

In this video, Tim Walsh (Siemens) and Marie-Teres Moser (University of Applied Science in Lucerne) provide a detailed look inside the technical setup of the Project PEARL in the Pilot Lab on the Siemens Smart Infrastructure Campus in Zug.

From airflow tracking with smoke and lasers to recovery time measurement and user comfort analysis, this 10 minute long session reveals how complex, high-precision data is gathered to evaluate laboratory ventilation system performance.

A peek into the results: Authentic data that reflect real-world performance conditions for labs

PEARL's independent testing reveals significant performance variations between lab ventilation systems, providing laboratory professionals with unfiltered data that reflects actual operational scenarios. Here are some of the remarkable data and results the PEARL Project was able to gain.

31% Superior local air change rate

Despite lower airflow speeds, the Smart Lab Ecosystem HL-X-VENT™ system achieved a 31% superior average local air change rates – proving that safety and contaminant control don’t require excessive airflow.

300 w/m2 - Masters extreme heat load variations

While most systems struggle beyond 180  W/m², the tests shows that the Smart Lab Ecosystem partner offering HL-X-VENT™ maintains user comfort even under high internal loads of up to 300  W/m².

29% Faster particle removal

In the center of the room (near fume hood), particle removal was 29% faster with the HL-X-VENT™ air and light channel compared to traditional laminar flow inlet diffuser – a critical safety factor for lab conditions.

45% Better ventilation efficiency

Ventilation efficiency measures air volume needed for a specific room condition. We measured less than half the air volume needed, achieving 45% better efficiency, demonstrating superior removal of dangerous gases and heat.

Next steps: The digital twin of PEARL

Project PEARL, conducted by the University of Applied Sciences Lucerne, has collected a wealth of valuable data. This data, analyzed in collaboration with Siemens experts and partners, forms a solid foundation for innovative projects and impactful use cases.

How to use the power of collaboration & simulation to enhance the future of labs:We created a digital model of Project PEARL that went beyond simple geometry. We modelled thermal and fluid dynamics, particle trajectories and factors impacting safety and comfort. When we compared simulation results to actual data from Project PEARL, the accuracy was remarkable. This capability is transformative. It allows us to simulate equipment loads and assess risks – such as high air velocities directly in front of fume hoods – before spending a single dollar on construction. We can adjust designs to optimize performance, safety and comfort all within the digital twin of your next-generation lab.