Skip to main content
This page is displayed using automated translation. View in US English instead?

A heritage ship protected by water

How do you protect a 20th century wooden training vessel in a museum full of irreplaceable objects? With water. In Milan, discreet high-pressure water mist fire suppression technology keeps one of Italy’s most precious heritage assets safe without changing how it looks or how visitors experience it.

Preserving irreplaceable maritime craftsmanship

The Ebe schooner, a former training vessel on display at the National Museum of Science and Technology Leonardo da Vinci in Milan, is a unique cultural artefact that needs special protection. A risk assessment conducted by fire engineering specialist Jensen Hughes revealed that a fire ignited by something as simple as an electrical fault could develop rapidly – faster than the fire brigade could be on site. This highlighted the need for a dedicated fire protection system.

Protection without a trace

Fire Suppression Reference Museo Leonardo Da Vinci

Designed to blend in

Lightweight, small-diameter piping allowed the Sinorix high-pressure water mist system to fit through narrow passages. Its discreet installation blends seamlessly into the surroundings and is barely noticeable to visitors.

Fire Suppression Reference Museo Leonardo Da Vinci

Water, intelligently used

The intelligent use of water protects in two ways: closed nozzles automatically suppress fires, while separate open nozzles gently humidify the wood to preserve its moisture balance.

Fire Suppression Reference Museo Leonardo Da Vinci

Proven technology

The Sinorix system installed on the Ebe has been successfully proven in full-scale fire tests, matching the risk profile represented by the training vessel.

Protection beyond standard requirements

Protecting a heritage object starts with understanding its specific risks.

For the Ebe, Jensen Hughes identified the specific fire risks and defined the protection requirements using a performance-based fire safety approach. Siemens provided the flexible Sinorix high-pressure water mist technology needed to address them. Together, they developed a bespoke solution that protects the vessel while respecting the museum environment. As Henrik Bygbjerg, Director of Testing & Approvals at Siemens, explains: “Fire protection strategies cannot rely on a single standard and may require application-specific considerations, unique to each project.”

Fire Suppression Reference Museo Leonardo Da Vinci rudder house
Fire Suppression Reference Museo Leonardo Da Vinci sideview

Protection and preservation all in one system

The Sinorix high-pressure water mist system isn’t just offering protection in case of an emergency; it helps preserve the Ebe all year round. Open nozzles without bulbs handle periodic, manually operated humidification inside the vessel, protecting the wooden structure of the ship from deteriorating. Closed nozzles with temperature-sensitive bulbs, installed on both sides of the ship’s compartments and externally, provide fully automatic fire suppression. And because each nozzle’s bulb triggers independently, only the one closest to the point of ignition activates. This keeps fire suppression targeted instead of flooding the whole compartment.

Protection designed to scale

The project shows how holistic fire suppression solutions can deliver value beyond traditional fire protection standards, by supporting life safety, property protection, business continuity and sustainability. The Sinorix high-pressure water mist system was designed with future scalability in mind, giving the museum the option to extend protection to other occupancies across the museum complex.

Bold black Italian lettering on a glass entrance door spells out