Skip to main content
This page is displayed using automated translation. View in US English instead?

So that nothing at all spoils the enjoyment of beer

Maisel & Friends is networking the fire alarm technology for the Liebesbier Restaurant and the new Urban Art Hotel and installing state-of-the-art technology that at the same time hardly touches the aesthetics of the rooms.

Brewing tradition meets modernity

Since 1887, the Maisel Brothers family brewery in Bayreuth has been brewing and producing the wheat beer speciality Maisel's Weisse or the modern Maisel & Friends beer specialities, among other things. The Maisel & Friends brewery site turns the craft into an experience. In the "Liebesbier Restaurant" there are more than 80 beers from the bottle and 21 from the barrel, plus dishes prepared with regional ingredients. With the "Liebesbier Urban Art Hotel", a smart hotel has been created that combines old buildings with modern architecture. A special highlight: All 67 rooms and the outdoor areas were individually designed by over 60 international street artists from over 30 countries.

Adapted to special needs

From the very beginning, the modernisation concept focused on the different uses of the buildings and the structural features of the listed old buildings. The potential fire and explosion hazards from the processing of highly flammable materials, such as alcohol and coffee powder, were a particular challenge. The show kitchen also required special monitoring due to the enormous heat and steam development. For the comprehensive protection of guests, staff and valuable technology park, the Sinteso fire alarm system was therefore installed.

For us, Siemens is a valuable partner to ensure that our buildings will continue to stand for the next 100 years.
Jeff Maisel, Owner and Managing Director, Familie Maisel GmbH & Co. KG

Meeting high fire protection requirements

7bb7ccdf-1f5f-4d23-b1b8-ba8c26fb3e56-referenz-maisel-and-friends-restaurant-1280x720

To ensure that people can be led quickly out of a possible dangerous situation, comprehensive detection and alerting in the various buildings is essential. In the hotel, restaurant, show kitchen, coffee factory, brewing workshop and the event rooms, theSinteso fire alarm systemfor monitoring and alerting. Automatic and non-automatic detectors and signal transmitters are used depending on the environment and networked in the various buildings.

b19f4fa4-e94a-4660-8e09-19d029952c63-referenz-maisel-and-friends-brauwerkstatt-1280x720

Thanks to the fire protection concept implemented by Siemens, Maisel & Friends can concentrate on its core business beverage industry. All areas are protected by the fire alarm technology installed and networked in the various buildings. This ensures operational safety on the entire site and creates the framework conditions for the greatest possible flexibility and productivity required in the catering and hotel sector. The coloured fire detectors used at the request of the operators blend discreetly into the ambience, so that the aesthetics of the rooms are hardly affected.

Safe ambience for leisure hours

6f282510-1e10-4585-8626-2df54283adcd-Referenz-Maisel-and-Friends-Bier-2-1280x720

Thanks to the fire protection concept implemented, Maisel & Friends can concentrate on what they can do: brew beer and score points with hospitality. Image: ©Maisel & Friends

684d3576-91f7-4d39-b52a-ea6a213e9ec4-Referenz-Maisel-and-Friends-Crazy-Sheep-1280x720

The aesthetics of the rooms are hardly affected by the technology. Image: ©michaelbauerphotography.de

f49690a1-a6c8-4b56-b0a9-5e38be1bbe0e-Referenz-Maisel-and-Friends-Liebesbier-Innenaufnahmen-Michael-Bauer-23-1280x720

With Sinteso, the family-owned company receives an all-round efficient and highly reliable fire protection system that creates a safe environment that protects people, processes and infrastructure. Image: ©michaelbauerphotography.de

More information

Fire protection

Protecting people, assets, and buildings—around the clock, 365 days a year. With cloud-based technologies and our many years of experience in the field of fire protection.

A graphic showing a factory with a focus on process optimisation using AI technology.

Food and beverage industry

Learn how digitalization and automation are making the food industry more sustainable.

Maisel & Friends

Maisel & Friends in Bayreuth is the place to go for experiences related to beer.