Skip to main content

Existing buildings on course for sustainability

Goethe University in Frankfurt am Main is one of Germany’s largest universities and aims to achieve net-zero carbon operations as soon as possible. The energy modernization of the Biocenter at the Riedberg campus shows how existing buildings can be efficiently upgraded for sustainability.

Efficiency and sustainability through energy upgrades

With around 48,000 students, five city locations and buildings over a century old, implementing sustainable operations requires comprehensive solutions. The recent modernization of ventilation and air-conditioning systems at the Riedberg campus shows the potential of targeted energy upgrades.

A modern building with a glass facade and a large entrance, likely a university or academic institution.

In focus: Biocenter at the Riedberg campus

Built in the 1990s, the Biocenter at the Riedberg Campus, which houses the natural sciences faculties, comprises seven buildings with a total area of around 71,000 square meters. Its annual energy costs have so far been in the single-digit millions. The main cause has been the outdated ventilation technology, which accounted for over 80% of heat consumption and more than 50% of electricity consumption. With a comprehensive plan for modernizing the energy efficiency of the ventilation and air conditioning systems, the university aims to reduce energy costs and CO₂ emissions in the interests of greater sustainability.

Impressive results

€ 236k annual energy cost savings

The first modernized building saved nearly two thirds of thermal energy and over half the electricity used by its ventilation systems compared to the previous year. Annual energy cost savings are estimated at €236,000.

50% subsidised by the state of Hesse

The project makes a significant contribution to the climate protection plan of the state of Hesse. It therefore received a 50% subsidy as part of the Hesse CO₂ reduction and energy efficiency program.

4 years until full amortization

The energy modernization of the ventilation and air conditioning systems will pay for itself in just a few years thanks to the energy cost savings that result from the increase in efficiency in combination with state subsidies.

The extent of the efficiency improvement and cost savings has significantly exceeded our expectations and shows the potential offered by energy modernization in existing buildings.
Gabi Lilienthal, Team Leader Technical Building Services, Goethe University Frankfurt

An end-to-end modernization plan

Together with Siemens and other project partners, Goethe University developed a comprehensive plan for the energy modernization of the Biocenter. Ventilation and air-conditioning systems and the measurement, instrumentation and control technology in buildings are now being modernized step by step.

Two men inspecting an open electrical cabinet with many wires and components.

Control cabinet modernization

Control cabinet modernization was structured to save space, with compact input and output modules in line with the current TX-IO standard. In conjunction with the new Desigo PXC automation stations, this leads to greater operational reliability.

A gloved hand in a lab coat adjusts a knob on a scientific instrument with colorful buttons.

Demand-controlled supply and exhaust air

Equipping the special exhaust air fans in the fume cupboards with EC motors and motors with frequency converters ensures demand-driven exhaust air functionality. The air exchange rates are adapted to the actual room requirements using demand-based control strategies for the supply and exhaust air systems and presence sensors in the laboratories.

A complex industrial room filled with pipes, machinery and a large blue tank.

Heat recovery

A newly installed heat recovery system was connected to the existing Desigo building management system via BACnet coupling.

Two men in an industrial setting, one pointing at a large diagram on the wall.

Accompanying services

A customized service package consisting of traditional maintenance and digital services together with professional energy data management is rounding out the energy modernization measures.

Students studying in a bright library, visible through an "X" shaped cutout on a dark blue background.

Make your campus an innovation hub

Siemens Xcelerator helps create efficient, secure and sustainable campuses and accelerate digital transformation.

Sustainability gains for your campus

The successful energy modernization of the Biocenter at the Riedberg campus highlights the many ways in which a university campus can increase efficiency and sustainability.

Are you also facing the challenge of developing existing buildings into more sustainable buildings? Let’s evaluate the options together and develop the strategies you need.

The team of experts: Thorsten Ambron (Project Manager, Siemens), Marco-Oliver Dittmar (Senior Sales Representative, Siemens), Gabi Lilienthal (Team Leader Technical Building Services, Goethe University Frankfurt), Jens Sommer (Systems Engineer, EBC)

The team of experts: Thorsten Ambron (Project Manager, Siemens), Marco-Oliver Dittmar (Senior Sales Representative, Siemens), Gabi Lilienthal (Team Leader Technical Building Services, Goethe University Frankfurt), Jens Sommer (Systems Engineer, EBC)