Skip to main content

Exceeding high expectations

For the construction of the new production hall in Schopfheim, Develco Pharma was looking for a consistent overall solution. Anyone who manufactures highly potent painkillers must offer a high level of safety, comprehensive fire protection and a special building automation solution for laboratories.

Everything from a single source – Desigo CC

Anyone who produces pharmaceuticals faces a high level of responsibility in terms of quality and reliability. Just like Develco Pharma GmbH. It manufactures pharmaceuticals for the treatment of severe pain (opiates) for the European and North American markets. Develco Pharma Schweiz AG was founded in 2006 and is now headquartered in Pratteln. Since 2017, painkillers and drugs for attention deficit deficits (ADHD) have been manufactured in a new production hall at the Schopfheim site in Germany.

An industrial ceiling with a fire alarm, a large silver ventilation duct with wires and sensors and a ladder in the background.

Challenge

For the construction of the new production hall in Schopfheim, Develco Pharma was looking for a consistent overall solution for special requirements. After all, anyone who manufactures highly potent painkillers must offer a high level of safety, comprehensive fire protection and a special building automation solution for laboratories. The solutions should be able to be monitored and operated by a higher-level management system.

Solution

Two aspects were decisive: the reliable solution from a single source and the management platform for all trades. All building technology trades come from Siemens. Our Desigo CC management platform monitors and controls the automation stations and operating devices from Desigo PX, as well as the laboratory solution, the intrusion alarm system, the access control system, the video surveillance system and the network-compatible fire alarm control panel. Special solutions are used for the laboratories, such as structure-borne sound and motion detectors or the recording of room conditions such as pressure, temperature and humidity.

A person in a white lab coat uses a stylus to interact with a Siemens industrial touchscreen display on a metallic control panel, with buttons below.
A cleanroom laboratory with various stainless steel and white machinery, including a large black and white unit, a smaller unit with a clear cylindrical component, and computer workstations behind a glass partition.

Benefit

We tailor the overall package for security, fire protection and building automation precisely to the requirements. It fully meets both the high demands of our customer and the official requirements. With Desigo CC, all trades in the building are centrally controlled and optimized. For the customer, everything from our source means: high production reliability, high operational efficiency and comprehensive service. This creates an ideal environment for sophisticated high-tech drug production.

All-around building technology solution

Icon Haken - original - cb13a5e8-c00b-4484-ac6b-ad31fc05a26c

Future-proof with Desigo CC

All systems can be centrally controlled, controlled and monitored with the building management platform.

Icon Haken - original - cb13a5e8-c00b-4484-ac6b-ad31fc05a26c

Technology for special requirements

All requirements are met with the Desigo PX building automation system, the CET laboratory automation system and the CMT monitoring system.

Icon Haken - original - cb13a5e8-c00b-4484-ac6b-ad31fc05a26c

Fire protection solution covers all cases

The Sinteso FC 2040 fire alarm control panel, together with multi-criteria detectors and the FDA241 smoke aspiration system, provides comprehensive and reliable fire protection.

Icon Haken - original - cb13a5e8-c00b-4484-ac6b-ad31fc05a26c

Security solution offers all-around protection

Security is provided by the Transliner CIC2010 intrusion alarm system with Sipass access control, MyTMA time processing and SiNVR video surveillance.