Growing fat to make plant-based meat alternatives tasty
The start-up Cultimate Foods sees itself as a part of this movement. “Basically, what we are trying to do in the long run is to get animals out of the food chain,” says Morales-Dalmau. Sure, restaurants, fast food chains and supermarkets are already full of plant-based meat alternatives. However, the problem is that, often enough, taste and texture are not satisfying to people who are used to eating “real” meat. Morales-Dalmau, who is vegan, admits: “Fat is a pleasure. It gives taste to the meat.” That is why, according to him, 64 percent of people who have tried plant-based meat alternatives will not try them again.
The producers are trying to tackle that problem by adding coconut or rapeseed oil – or artificial flavors, which make the product less healthy. “In the end, what makes meat tasty, when you cook it, is the fat,” says the Catalunya-born Spaniard, who started as a theoretical physicist, then made his way through cancer therapy research, before switching to food technology in 2022.
Hybrid patties for climate-conscious meat lovers
Morales-Dalmau and his colleagues extract live cells from cows and pigs; then isolate, expand and differentiate them, which basically means that they instruct them to cultivate fat inside. The main attraction is that the cultivated fat will be healthier than conventional fat: “What we are cultivating aren’t subcutaneous, but intramuscular fat cells, which have less saturated fatty acids,“ says Morales-Dalmau.
The cultivated fat is then added to different types of plant-based meat alternatives. And then the team – since this year a group of eight – does tastings. Morales-Dalmau takes out some plastic bags filled with a mixture from the fridge that resembles minced meat. The week before, for the first time, they moved their product from the lab to the plate, doing burgers with their “hybrid patties”. Cultimate calls its product “hybrid” because the final product is a mixture of plant-based product and lab-grown fat. The product may not appeal to strict vegans but they might convince customers who want to reduce their consumption of animal-based meat.
Cultivated fat can be added to different types of plant-based meat alternatives.
For example, "hybrid" sausages could be produced.