Skip to main content
SENTRON arc fault detection devices from Siemens

Understand AFDD switches — simply and effectively

Electrical arc faults pose a serious fire risk. Explore the technology behind arc fault protection, relevant safety standards and how SENTRON Arc Fault Detection Devices (AFDD) address the root cause of electrical fires by detecting dangerous arcs and interrupting current flow instantly.

What are arc faults?

An arc fault occurs when electrical current jumps through the air, creating a fire hazard by easily igniting nearby flammable materials.

There are several causes:

Series arc faults occur when there is a break in a single wire due to damaged insulation, pinched wires or loose contacts — often without overcurrent or fault current.

Parallel arc faults occur when adjacent conductors, such as phase and neutral, come into contact due to pinched cables.

The image shows a modern building with a sleek design, possibly a Siemens Evaluation and Testing Center.

Detecting and interrupting arc faults with AFDDs

Protection mechanisms in practice

In electrical installations, short circuits, residual currents and arc faults create multiple risks. For continuous cable protection, personal safety and preventive fire detection, you need several protective components that work together:

  • Residual current devices (RCDs) continuously monitor the current flowing in live and neutral wires. If they detect even a small difference, they instantly cut the power
  • Miniature circuit breakers (MCBs) offer protection against overload and short circuits
  • AFDDs detect arc faults to help protect against resulting fires

AFDDs from the SENTRON portfolio provide reliable detection of series and parallel arc faults. They immediately interrupt the current flow — even in situations where conventional protective devices fail.

A diagram showing different types of protective enclosures for electrical equipment.
A Siemens advertisement featuring a person in a blue shirt and a blue background with text.

Space-saving installation of AFDDs

In modern electrical installations, available space in main distribution boards, sub-distribution boards and switchgear assemblies is often limited due to the increasing demand for control, communication and safety technology. However, thanks to the compact design of Siemens’ AFDDs, you don’t have to sacrifice preventive fire protection due to lack of space.

Siemens has developed a special AFDD variant that is also ideally suited for retrofitting an arc fault detection device in existing installations: the SENTRON 5SV6 AVDD. It can simply replace the existing miniature circuit breaker, as it has an MCB already integrated. In addition, you can retain your existing pin busbar system.

SENTRON AFDDs flexible application

The SENTRON 5SV6 combines AFDD and circuit protection in just one modular width (MW), ideal for both new installations and retrofitting. This means standards-compliant expansion is possible without requiring any additional space.

You can implement complete protection within just 2 MW using the SENTRON portfolio:

AFDD (SENTRON 5SM6) for fire protection

RCBO SENTRON 5SV1 for personal and cable protection

The RCD function is available with 30 mA or 300 mA, while the MCB function is available with B or C tripping characteristics.

The SENTRON 5SV6 is ideal for flexible use cases such as older residential buildings, kindergartens, care facilities or offices with high load distribution, which are particularly susceptible to electrical fires.

Two Bosch vacuum cleaners, one blue and one white, standing upright on a light background
Grafik-Gebaude-Brandrisiko-640x480

AFDD standards and responsibilities

DIN VDE 0100-420:2019-10 defines fire protection requirements for electrical installations in buildings, including power distribution systems. It recommends using AFDD in final circuits in the following locations:

  • Rooms and locations with combustible building materials (fire resistance class below F30)
  • Rooms with sleeping accommodation (regardless of building materials)
  • Rooms and locations with a risk to irreplaceable assets
  • Rooms or locations with a particular fire risk according to the Model Building Code (MBO § 2.19)

If an AFDD is not installed in these locations, the standard requires a documented risk and safety assessment, which can be complex and time-consuming. Using an AFDD from the SENTRON portfolio is a simpler and safer solution.

Discover the SENTRON portfolio

See how Siemens products can help you protect your electrical systems.

SENTRON arc fault detection device

SENTRON arc fault detection devices (AFDDs)

Detect all types of arc faults with AFDDs from the SENTRON portfolio. Learn more about why SENTRON AFDDs are essential to help protect your building against fires.

SENTRON miniature circuit breaker

SENTRON miniature circuit breakers (MCBs)

Easy to install and flexible for a wide range of applications, MCBs from the SENTRON portfolio can help protect your electrical system against overload and short circuits.

A Siemens powerpoint slide with a visual representation of a power system and a diagram of a power supply system.

SENTRON residual current protective devices (RCDs)

RCDs from the SENTRON portfolio are a compact solution for residual current and line protection, breaking the current immediately and safely in the event of an arc fault.

เริ่มต้นการเดินทางของคุณ