Skip to main content

Upgrading fire safety in a Rotterdam skyscraper

The 165-meter-high Maastoren accommodates 1,800 to 2,500 workers daily and stands as the Netherlands' second-tallest building. What happens when you need to replace the entire fire safety system while the building remains fully operational?

This complex challenge became reality during the modernization of the fire detection and evacuation system of the Rotterdam skyscraper. The Maastoren was completed in 2009 and has since become one of Rotterdam's most iconic office towers. From the top floor, you can see the entire city, the Maas River, and the port. Verkerk Installatietechniek designed and implemented the complete electrical installation at the time, including the fire detection and evacuation systems.

After more than 15 years of reliable service, the first signs of aging began to show. The issues were both technical and functional. "The installations functioned well for years, but eventually we ran into limitations," explains Henk Vastenburg, technical coordinator. "Certain components were no longer available, and we received complaints about the high-pitched tone of the evacuation system."

Finding the right solution

As manager of the Maastoren, Savills Netherlands worked with the building owner and Verkerk to find a future-proof replacement solution that would align technically and operationally with the building's needs. Various systems were evaluated for reliability, business continuity, and expandability. Based on this evaluation, Paulo Dias, technical manager at Savills, chose our Siemens installation on behalf of the owner. Our solution provides a modern and reliable foundation for the coming years and also aligns with the building's sustainability and management objectives. "With this investment, we are not only replacing an outdated system, but above all choosing a safe, future-proof, and efficient solution for our tenants and users," says Paulo.

More than just technology

We supported the project through Patrick van den Heuvel, who helps building owners and installers design fire safety solutions at Siemens. He was involved in the design and configuration of our Cerberus fire detection system and the Novigo type A evacuation system.

"We visited the site multiple times to properly understand the situation," explains Patrick. "In projects like this, it's crucial that you don't just look at the technology, but also at how the building is used. Only then can you create a design that actually works in practice." This collaboration between manufacturer and installer proved essential. Stefan Dommers, client manager Safety & Security at Verkerk, puts it this way: "We have extensive knowledge in-house, but with an installation of this scale and complexity, you need the manufacturer's expertise to properly coordinate everything."

Article block - Maastoren fire safety system modernization - more than just technology - image

Cooperation between the manufacturer and the installer is essential to create a design that works well in practice for an installation of this scale and complexity.

Replacement without disruption

Besides the engineering, the execution was also challenging. The Maastoren remained fully operational throughout the entire project. Tenants continued working, visitors came and went, and safety could never be compromised. This meant: phased replacement, careful planning, and continuous coordination. "We started with the evacuation system," explains Maurice van der Horst, field service engineer at Verkerk. "This is controlled by the fire detection system, so everything had to connect perfectly. We worked floor by floor, with the new evacuation system temporarily remaining connected to the old fire detection system. This way we worked our way up, from the 1st to the 45th floor."

Digital fire panel for faster emergency response

maastoren fire safety system modernization - Digital fire panel - image

2 to 3 floors were tackled daily. No major interventions all at once, but controlled steps in a complex system. Subsequently, Verkerk installed the new FDS and connected it to the evacuation system. According to Maurice, this was a considerably complex phase of the project. The existing fire panel had to remain operational, and the alert transmission to the fire department was temporarily connected in parallel. "Those kinds of choices aren't visible to the user," says Maurice, "but they're essential for continuously guaranteeing safety."

The existing fire panel was ultimately replaced by a digital fire panel connected to the fire detection system via BACnet (Building Automation and Control Networks) communication protocol. This connection ensures that current fire alert information is directly available to emergency services and contributes to rapid and effective incident response.

Smart detection: fewer false alarms

The new fire detection system consists of 8 fire detection control panels. 6 of these are distributed across the building's vertical shafts. Additionally, 1 control panel is placed in the basement and 1 on the ground floor. In total, approximately 1,700 optical detectors were installed. In break rooms and kitchenettes, our detectors were used that can distinguish between real smoke and things that mimic smoke, like steam from hot water. This reduces the chance of false alarms.

We also paid special attention to preventing unwanted alarms in the stairwell and parking garage. These are public spaces where smoking sometimes occurs, which can lead to false alerts. Therefore, detectors were installed that are resistant to such environmental influences. Thanks to these smart choices, our system detects fire quickly and reliably, while minimizing unwanted alarms.

Targeted evacuation with spoken instructions

2 compact control panels on the 3rd floor and 2 large, modular control panels on the 29th floor together form the heart of the new evacuation system. An average of 45 speakers are placed per floor. This allows the building to be controlled in a targeted manner during an incident. Instead of a generic evacuation, each floor works with spoken instructions.

By evacuating in a targeted manner, the situation remains manageable, even with large numbers of people. The annual evacuation drill shows what this means in practice. Within just over half an hour, a large part of the building can be evacuated in a controlled manner, without panic and with clear direction toward the assembly point on the quay. During the replacement work, Verkerk's team experienced such an evacuation drill, allowing them to experience the operation of our installations directly in practice.

Remote monitoring

Through our Fire Manager application, Verkerk can remotely monitor the Maastoren's fire safety installations. Instead of reacting to malfunctions, the focus is increasingly on looking ahead. "For example, we can read out the contamination level of detectors," explains Nico Bloem, digitalization project manager. ""This allows us to know in advance which detectors need extra attention during maintenance. This makes it possible to plan work in a targeted manner and execute it faster."

Our system provides continuous insight into the installation's status. This allows checking whether all components are correctly activated and functioning as intended. "A while ago we received a notification that part of the installation was switched off," continues Nico. "We immediately contacted Henk. He indicated that this was done intentionally due to diving work around the building. Thanks to this monitoring, we can act proactively and sometimes even respond earlier than the customer themselves."

Digital testing for faster maintenance

Technicians can test detectors while walking through the building using our app. Results are directly recorded in a digital logbook. This prevents errors, speeds up the process, and ensures current data. Although Henk can also use the app, he still prefers a more direct communication line. "When something comes up, I call security directly. That works best for us."

Henk is satisfied with the end result. "The new installation is more user-friendly than the old one, which simplifies daily management."

October 2026