Skip to main content

Turn pharma infrastructure into an advantage

Align power, utilities and environmental controls with the output your site must deliver. Identify constraints before expansion, reduce avoidable energy use and operating costs and prepare the facility for changes in products, equipment and production demand.

Make installed capacity usable capacity

A production line can be available while utility constraints limit its output. Siemens brings power infrastructure, building controls and energy management into the production plan to help teams:

  • Assess electrical and utility demand, including operations that need the same supply at once
  • Maintain the environmental conditions required by the process
  • Identify avoidable energy use and opportunities to reduce costs and emissions

Support output at a sustainable operating cost

Icon of a dark blue and light blue thermometer with temperature readings on the outside of the thermometer

Protect the output planned for your investment.

Assess simultaneous electrical and utility loads alongside production schedules so infrastructure constraints are addressed before they leave installed equipment underused.

Icon of a blue leaf with the stem at the bottom left and head to the upper right

Maintain the conditions required for production.

Use monitoring, controls and records suited to each cleanroom, laboratory or manufacturing area. Connect environmental performance with the process it supports.

Icon of a dark blue computer monitor with light blue graph and bars indicating analytics and results.

Reduce avoidable energy use and utility costs.

Compare consumption with production demand to identify inefficient equipment and unnecessary use. Evaluate improvements against the conditions required for product quality.

Plan and operate the facility as part of production

Assess utility constraints before expansion

A new line may add demand for purified water, steam, cooling and electricity. Evaluate capacity against the production schedule, including operations that compete for the same utility. Assess these loads alongside equipment and material flows so expansion decisions reflect the output the whole site can support.

Infographic image of two scientists working in a lab with vials and a telescope

Relate environmental conditions to the process

Temperature, humidity or pressure deviations can affect production and trigger an investigation. Match monitoring, controls and records to the intended use of each area. Linking facility conditions with process context helps teams determine what changed and assess the consequences for the affected operation.

Infographic image of scientist in cleanroom working on tablet with vials, machines, and cleanroom technology

Reduce energy use while maintaining required conditions

Monitor energy and utility consumption against production demand to identify inefficient equipment or avoidable use. Evaluate proposed changes against environmental and process requirements before altering operating settings. Lower consumption is useful only when the facility continues to maintain the conditions required for product quality. Assess electrification against energy supply and emissions goals.

Siemens Building X Energy Manager analytics dashboard with charts and graphs

Prepare the facility for credible future needs

A new therapy or equipment upgrade can alter containment, cleaning, environmental and utility requirements together. Preserve engineering knowledge to evaluate those dependencies before making changes. Plan adaptability around likely future uses, including qualification needs, to avoid unnecessary complexity and reduce later rework.

Infographic image of Life Sciences Smart Lab Ecosystem with scientist looking through microscope