Skip to main content

SolarReady™ Meter Combo Recall

Recalled Product: Siemens SolarReady™ Meter Combo Catalog Numbers MC2442S1200SC and MC2442S1200FC.

Contact us for further instructions

Recalled Product: Siemens SolarReady™ Meter Combo Catalog Numbers MC2442S1200SC and MC2442S1200FC.

Period of Supply of impacted Product: Products were supplied nationally from August 1, 2021, through August 31, 2022.

Hazard: A wire with an incorrect stripping length may have been applied in the internal assembly, which allows for a lug set screw to compress the wire insulation instead of the conductor alone. This can create a poor electrical connection, resulting in overheating within the product and a risk of fire.

What to do

Homeowners:
Please use these instructions to determine if further inspection is required. If you need assistance following these instructions, please contact Siemens Electrical Products at: 1-800-756-6996 or psn.industry@siemens.com.

Professionals:
If you have information on where panel(s) may be located, please contact Siemens Electrical Products at: 1-800-756-6996 or psn.industry@siemens.com.


Contact us for further instructions

How to identify if you have an affected product

Siemens Solar Ready Meter Combos MC2442S1200FC and MC2442S1200SC have a label on the inside of the right panel door. This is where you can find the catalog number and manufacturing date stamp. Please refer to the Identification Instructions for more information. 

A tall gray electrical panel is open, showing a round component, labels, and an orange-marked area with illegible details.

Product Label

This photo is an example of what the label will look like. In the top left corner of the label, there will be a catalog number beginning with “MC”. At the bottom of the label, there is a black ink stamp with a manufacturing date. Please refer to the Identification Instructions for more information.

A Siemens technical specification sheet with a diagram or chart and the date “AUG 03 2022”.