Skip to main content

Smart energy management for greater resource efficiency

Sustainability is becoming increasingly important in industry. 20 percent of CO₂ emissions are created by industry. And 38 percent of energy consumption is attributable to industry. Due to rising energy prices and scarce resources, companies are under great pressure to counteract these conditions.

A strong partner for zero emission mobility technology

The automotive supplier ElringKlinger has recognized the urgency of the issue and is fully committed to sustainability. For example, ElringKlinger is the first Tier 1 supplier to offer its own integrated drive train for electric vehicles consisting of an electric drive unit, battery, and fuel cell. In addition, there is the first series production of fuel cells based on e-fuels in Germany. This expertise is also appreciated by Airbus, with whom ElringKlinger is jointly developing a fuel cell for aircraft.

Improve energy efficiency

Thanks to holistic energy management, key energy efficiency figures can be displayed and analyzed, and optimization measures be initiated to improve the energy efficiency of their plants. This also fulfills legal requirements.

Optimize load management

ElringKlinger produces its own energy, first in the form of waste heat and second as solar energy to increase its resource efficiency. This energy can be integrated into balancing load management and reduces costs.

Take data-driven steps toward decarbonization

Emission monitoring and control is conducted as part of energy management. It measures CO₂ emissions, determines the CO₂ footprint for each product, and thereby creates all the conditions for minimizing this footprint.

CO₂-neutral by 2030

In keeping with its pioneering role, ElringKlinger AG has set itself an ambitious goal: The company aims to achieve CO₂-neutral production in Europe by 2025 and in the USA and Asia by 2030.

Andreas Weiss, CU Vice President of Quality & Sustainability Management, is convinced: "Some people think sustainability and environmentally friendly production are some kind of luxury: but these are hard-core, entrepreneurial factors, creating money that literally flows through any company. You either do something with it or just let it flow away."

ElringKlinger "does something with it." However, this also implies mapping the entire carbon footprint of all products in all plants worldwide. Such an ambitious project requires a strong partner – which ElringKlinger has found in Siemens.

Andreas Weiß, CU Vice President of Quality & Sustainability Management

Uniform energy management

Working with ElringKlinger, Siemens designed the company's digital transformation, which consists of the three aspects digitalization, automation, and standardization and is scalable to all plants worldwide.

Man sitting in front of a monitor showing locations across Europe on a map next to performance data

Digitalization and automation are integral parts of a digital enterprise that can master current challenges, such as more individual product development with scarcer resources. Digitalized and automated processes ensure faster, more flexible, and more efficient production. Standardization lays the groundwork for implementation: It reduces the complexity of the overall plant architecture and simplifies the integration of machines and systems. The result: Engineering time is reduced, plants are commissioned faster, process changes are implemented more quickly, and products are launched on the market in less time.

S7 EE Monitor and Energy Manager for real-time analysis

ElringKlinger was able to implement a uniform energy management system thanks to the extensive standardization of its plants. A team consisting of Thomas Haug and Daniel Scheurle from ElringKlinger and Torsten Maskos from Siemens worked together to identify the company's needs and devised a concept comprising a variety of hardware and software solutions. Here are a few examples: Sentron measuring devices and Simatic S7 EE Monitor (predecessor of WinCC addon ResCON- Machine efficiency monitor) are used for recording, visualization, and standardized efficiency evaluation of machines, energy flows, and consumption. Simatic Energy Manager analyzes and evaluates the data.

Two employees looking at a monitor with a chart
SIMATIC Energy Efficiency Packages (16:9)

The comprehensive energy management system was implemented using standardized Energy Efficiency Packages that can be ordered, making it easy to scale and implement the solutions. Now an energy analysis in accordance with the VDMA standard can be performed to provide information on energy consumption and energy efficiency on a large scale. Daniel Scheurle, Energy and Sustainability Manager at ElringKlinger, is impressed by how extensively energy can be recorded both locally and globally. He is also enthusiastic about the flexible graphical representation in the dashboard of the installed Energy Manager Pro: "Now I can view the enormous amount of data in real time in an analyzable way. Not to mention that this type of energy management can also be used to determine the carbon footprint of all our products. That’s a major step on the path to CO₂ neutrality.”

Increasing efficiency, reducing costs, saving resources

An important step on the path to sustainable production is to optimally use resources. Thanks to the implemented solutions, ElringKlinger achieves comprehensive data transparency that’s used to create a concept for the generation, storage, procurement, and use of energy: and that’s holistic energy management.

It marks another milestone in the mapping of our products’ carbon footprint. It allows us to virtually map an important aspect of our products: sustainability.
Andreas Weiß, CU Vice President of Quality & Sustainability , ElringKlinger AG