Skip to main content

Giving ice hockey players the edge that they need

ELITE Blade Performance Technology takes cutting-edge technology to the ice. Control systems ensure consistent and reliable sharpening that lets players perform at their peak.

Geared up for peak performance

In Canada, hockey is not just a game – it’s serious business and a huge part of the national identity. More than half a million registered Canadian players play on 2,860 indoor rinks and 5,000 outdoor rinks.

So, what’s the secret to a player’s speed, agility and control? The answer lies in the shape, or profile, of the skate’s blade. While it might appear flat, a skate blade has a curve, or combination of curves, from toe to heel that determine the balance between agility and power. And, each player has their preferred blade profile that helps them maneuver best.

ELITE Blade’s system makes it easy to sharpen hockey blades. Place the skates on top of the machine, choose the sharpening parameters on the computer panel, et voilà – the blades are sharpened to a player’s exact specifications.

Delivering precision, reliability and consistency

Canada customer stories elite blade skates bottom

Shaping and sharpening with ELITE Blade

Like all sharp edges, skate blades dull over time. Sharpening gives them new life. Traditional sharpening techniques, however, can alter the blade’s profile and impact player performance.

This is the problem that Elite’s founder, Denis Proulx, was looking to solve for his son, a player in the Quebec junior system. Denis Proulx’s frustrated search for a provider who could sharpen blades without degrading their profiles eventually led to him inventing a state-of-the-art computerized sharpener that could perfectly preserve the blade shape. That was the launch of ELITE Blade Performance Technology.

Cutting-edge technology for elite players

“Our system is used by more than 85 professional hockey teams in North America,” says Brian Baxter, President of ELITE Blade Performance Technology, “including the NHL, AHL, NCAA, Major Junior, and the new Professional Women’s Hockey League.”

“There’s been a great advancement in the knowledge of how minute changes in the shape of the blade affect skating style and skating performance,” Brian Baxter adds. “When we transitioned our sharpening systems from an analog system to a digital system, what we required was a digital control system, which allowed us to read the shape of the blade and then program the speed and pressure of the pass to perfectly preserve the profile.”

A man is using one of ELITE Blade’s revolutionary sharpening machines to sharpen skates.
A Siemens Unified Basic Panel that makes the machine easy to operate

Controlling for precision, consistency, reliability

ELITE Blade’s cutting-edge solution includes state-of-the-art technology from Siemens. “Our solution brings precision, reliability, repeatability, and consistency,” says Terry Raposo, Sales Account Manager, Siemens. “The control system, which includes the SIMATIC HMI Unified Basic Panel, the SIMATIC ET 200SP controller and SINAMICS S210 servo drives, helps the system achieve the precision needed on each sharpening.” A unified basic panel makes it easy to operate the machine. An RFID system keeps track of usage, performance and condition and gives a high level of traceability throughout all processes.”

Achieving better results for the players

Making sure that the Montreal Canadiens’ players have everything that they need to remain on top of their game is Pat Langlois, the team’s Head Equipment Manager. “Hockey is special,” he says. “My job consists of making sure the players get everything they need. There’s a lot of work involved with the skates. We have a 23-player roster, and each player uses sixteen sets of blades.”

Using ELITE Blade’s system has made Pat Langlois’ job a lot easier. “The most important thing for me is consistency,” he adds. “We have better tools to work with, to give better results to the players.”

An ELITE Blade sharpening machine is positioned in a workshop.
The most important thing for me is consistency. We have better tools to work with, to give better results to the players.
Pat Langlois, Head Equipment Manager, Montreal Canadiens