Passer au contenu principal

Compensation of Supervisory Board members

The regulations for the compensation of the members of the Supervisory Board are set out in Section 17 of the Articles of Association of Siemens AG.

The Annual Shareholders’ Meeting of February 12, 2026, most recently resolved on the compensation system and the provisions of the Articles of Association regarding the compensation of the Supervisory Board members, with a majority of 97.04% of the valid votes cast.

The compensation system as resolved, as well as the wording of the amendments to the Articles of Association, can be found under agenda item 7 of the Notice of the 2026 Annual Shareholders’ Meeting.

The amended provisions of the Articles of Association shall apply for the first time as from October 1, 2025.

The previous compensation system for the members of the Supervisory Board, which was resolved by the Annual Shareholders’ Meeting on February 3, 2021, with a majority of 97.49% of the valid votes cast, and confirmed by the Annual Shareholders’ Meeting on February 13, 2025, with a majority of 98.02% of the valid votes cast, can be found in the Notices of the Shareholders’ Meetings 2021 and 2025 under agenda item 7 and 8 respectively.

Siemens Management

Compensation of Managing Board members

Compensation reports