Skip to main content

Cybersecurity in Automation Solutions for Industry

NTO Automation has introduced an extra-layer security solution between the IT and OT network during the construction of a new factory for a major industrial client. Increased focus on cybersecurity in industrial automation helps eliminate access from the OT to the IT layer.

Security is a High Priority

Security was one of the crucial parameters when the automation solution for a new factory for a large Danish industrial company was up for tender. Data from automation forms the basis for financial transactions with the company's customers, so it is just as important to protect the OT network from internal attacks as it is to guard against hacker attacks and viruses from the outside. NTO Automation from Ikast won the tender.

"Most IT departments don't consider that when a programmer sits down and programs a PLC, that person could hack into the IT system from there. We've closed off that possibility with the way we've designed this system," says Kurt Nordholt, Key Account Manager at NTO Automation.

Two laptops appear at the top; green-outlined server equipment and computer monitors are also present.
Jann Storm Jensen, software engineer at NTO Automation

Jann Storm Jensen, software engineer at NTO Automation

Sharp Separation between OT and IT

The system is designed with a very strict separation between the customer's OT and IT networks. The solution is built in three layers, with a layer inserted between the IT and OT systems, known as a DMZ layer. DMZ refers to the military term "demilitarized zone," and every request to the customer's automation solution must go through a jump station located in the DMZ zone. From there, the request goes via a VPN to the OT layer, where each PLC is further protected by a firewall.

The solution is built according to the international security standard IEC 62443, and one way NTO has blocked unintended traffic is through so-called hardening.

"We have used hardening on all switches, which means that everything not needed is turned off. By default, everything is blacklisted. If the customer ever needs to connect a new component, we have to activate the protocols first. So you can't just come by and connect your own equipment to the network anywhere," says software engineer Jann Storm Jensen from NTO Automation.

Siemens is Best for Industry

NTO Automation has built the entire system with Siemens components. Communication is handled by a SIMATIC Soft PLC, and all control takes place on a decentralized PROFINET. The entire network from DMZ to OT is redundant, and the OT layer is built from several redundant rings, where data traffic can switch direction in less than 200 milliseconds.

"We chose Siemens because they have the best equipment for industry. They provide industrial products suitable for an industrial environment and can offer the complete security package with firewalls. While others think about selling some switches or components, Siemens is the only one who presented us with this way of building a secure OT network,” says Kurt Nordholt.

Kurt Nordholt, Key Account Manager at NTO Automation.

Kurt Nordholt, Key Account Manager at NTO Automation.

Resonates with Siemens Account Manager

This statement is received with both joy and recognition by Lars Henrik Jensen, account manager at Siemens.

"At Siemens, we have an enormous focus on cybersecurity within OT. In recent years, we have seen some terrible examples of what hacker attacks can mean for the finances of large companies, and especially in older installations, there is a risk that the production systems are not well protected. If we combine this with the entire development within Industry 4.0, where production and administration data need to flow more freely, it is extremely important to have control of security in operational technology," he says.

Lars Henrik Jensen is also pleased to have contributed to the development of the extremely secure installation.

"Siemens' role in the security part has primarily been as a consultant, where we have assisted in how the solution should be made according to the security standard IEC 62443. It is always a pleasure to help push the boundaries of security together with talented people," he says.

NTO has also not been the only supplier to the new factory. There have been other suppliers involved in the various sub-systems in the factory. All their units are now also encapsulated behind a PLC with a firewall.

Lars Henrik Jensen, account manager at Siemens

Lars Henrik Jensen, account manager at Siemens

"The other suppliers also have to go through our jump station to access their components. But we managed that well, and we've also had good cooperation with the customer's IT department," says Kurt Nordholt. Besides security, it was also important for the customer that administrative staff can freely collect the data they need for statistics and optimizations, and the solution does not prevent this.

Four Tablets for Two Floors

The customer’s new factory is on two floors, and as you move around the factory you will see driverless trucks, AGVs, controlled via a wireless network from Siemens routers.

The automation system's many components can be operated via four tablets placed throughout the factory, meaning operations can be managed by only two people. Maintenance of the network and SCADA is handled by NTO through a service agreement, as the end customer prefers to leave security maintenance to the experts.

DI webinar Big text

Explore Our Series of Webinars on Industrial Security

All webinars can be watched on-demand whenever it suits you.