Skip to main content

Revolutionizing industrial heat production

Guangzhou Nengyin Heat Pump Technology Co., Ltd.

Guangzhou Nengyin Heat Pump Technology Co., Ltd

Located in Guangdong Province, Guangzhou Nengyin Heat Pump Technology Co., Ltd. is a leader in high-temperature heat pump innovation. From its base in Foshan City, Nengyin is dedicated to developing efficient, high-performance heating technologies. Siemens has been a key partner for over a decade, committed to Nengyin's mission to revolutionize the high-temperature heat pump sector with groundbreaking solutions. Together, we are pushing the boundaries of industrial heating, setting new industry standards, and leading the way in sustainable solutions.

Challenges

In their quest to lead the high-temperature heat pump segment, Guangzhou Nengyin Heat Pump Technology Co., Ltd. faced some challenges. The primary pain point was the need for technological innovation that would ensure maximum efficiency and reliability in their heat pump applications, particularly in developing reliable solutions for high-temperature operation while optimizing system design for safety and efficiency.

A large, green and white industrial heat pump unit stands prominently in a spacious factory setting. The unit features intricate white grilles over blue cooling fins. In the background, other factory equipment and yellow work tables are visible under a high ceiling with exposed beams
Image of a siemens product: Refrigeration valve MVL702 and driver<br/>

Solution

In response to the challenges, Siemens embarked on a close collaboration with Guangzhou Nengyin Heat Pump Technology Co., Ltd., crafting a tailored solution to meet their specific needs. Instead of a one-size-fits-all approach, Siemens developed a bespoke total solution that includes the following components:

  • MVL702 magnetic expansion valve: higher operating temperature limit (Max. 130℃), accurate flow control, speed and valve accuracy to save energy by adapting superheat to lowest level yet stable operating point.
  • Climatix C400 controller: sharpens precision in system management.
  • Custom control application: tailored software that integrates seamlessly with existing technologies, honed to match Guangzhou Nengyin’s unique control logic and specific operational requirements.
  • Steam pressure and temperature sensors.

This customized approach not only meets but also exceeds the rigorous standards required, ensuring optimal performance and reliability.

How the solution helped solve customer’s challenges

In transformative pilot tests within Nengyin's state-of-the-art laboratory, the Siemens tailored solution marked a significant leap in performance.

A screenshot of the Climatix IC web interface displaying a 'CompRatio' trend graph. The graph shows two lines, red and green, fluctuating between approximately 5.00 and 9.00 on the Y-axis over a time window from 5:00 PM to 8:00 PM on September 29, 2024. Below the main graph, a green filled area graph shows 'Unit1.DispStatus.CompRatio2' over the same period. The interface also shows navigation options like 'Plant dashboard,' 'Data points,' and 'Alarms

180% High COP (coefficient performance)

An impressive 18% boost in COP during heating phases, outshining competitor benchmarks.

130°C Operations

Elevated temperature capability, enabling operations 130°C, positioning customers as leaders.

20 min Discharge superheat control

A groundbreaking acceleration in achieving target superheat, 3 times faster — 20 min instead of 60.

7.1 Compression ratio

Superior efficiency, showcasing a notably lower compression ratio of 7.1 compared to the competitor's 7.5.

Customer benefits

Nengyin achieves a competitive advantage through Siemens' advanced system, pushing their industrial heating beyond 130°C while maintaining energy efficiency. This results in significant energy cost savings and reinforces Nengyin's dedication to environmental sustainability.

A teal thermometer icon showing '130' in its bulb, next to a teal upward-pointing arrow, all on a black background. This indicates increased temperature capability.

Elevated Temperature Capability

Enables operations above 130°C, positioning customers as leaders in high-temperature applications

Icon of plug with cord circling a leaf illustration energy efficiency

Energy Efficiency with COP increase of 18%

Our technology significantly cuts operating costs and environmental footprint for end-users.

A green target with three concentric circles has a green arrow intersecting its center.

Strategic Partnership

Empowers our customer to achieve their goal of industry dominance with advanced, energy-efficient heat pump solutions.

The test results have validated the tangible benefits of the solution in enhancing the overall performance of high-temperature heat pumps. It fully meets the stringent requirements for such high-performance heat pump applications.
Mr. Lin Chunwen, General Manager, Guangzhou Nengyi

Aloita matkasi