PADS Pro Essentials
PADS Pro Essentials delivers affordable PCB design for independent engineers. The software provides professional-grade tools, easy digital access and community-based support.
Start where you need. Scale when you’re ready. The Xpedition family grows with you.
From independent engineers to global organizations, the Xpedition family is a fully integrated, scalable PCB and electronic systems design platform that helps teams design right the first time, validate earlier, and deliver cleaner handoffs from design to manufacturing, without re-platforming as complexity grows.
Systems and PCB design complexity has outgrown point tools and “throw it over the wall” handoffs. The teams that win aren’t just faster at layout – they are better at preventing respins by keeping the why (design intent), the how (constraints), the what (components), and the can we build it? (verification + DFM) continuously connected from concept through release. Xpedition is built for that connected reality: an integrated, scalable platform that helps teams move quickly without sacrificing engineering confidence as complexity and collaboration needs grow.
PCB programs break down when intent is scattered across files, tools, and people – constraints drift, libraries diverge, and “tribal knowledge” becomes the only way to understand why something was done. Xpedition is designed as an integrated environment where schematic, layout, constraints, libraries, and downstream deliverables stay aligned, so the why behind decisions is easier to preserve and the how is easier to enforce as the design evolves.
What this looks like in practice: fewer translation steps, fewer mismatches between domains, and a workflow where changes are easier to manage without losing confidence in the data.
With today’s edge rates and power density, waiting until the end to validate SI/PI (and other checks) turns verification into a schedule risk multiplier. The best-practice approach is digital-prototype driven verification – checking progressively as you design so you can make the big tradeoffs early, when the design is still flexible. Xpedition supports that shift-left mindset so verification becomes part of convergence, not a gate at the finish line.
What this looks like in practice: issues are exposed when fixes are cheaper, iterations tighten, and signoff becomes confirmation – not discovery.
Manufacturing questions, DFM escapes, and documentation churn are rarely “manufacturing problems” – they are symptoms of a late feedback loop. Xpedition supports concurrent DFM and manufacturing-aware checks so many issues can be identified and resolved while you’re still designing, not after release. It also supports intelligent manufacturing data exchange (e.g., ODB++ / IPC-2581) to reduce ambiguity and minimize errors that come from translating outputs or reinterpreting intent downstream.
What this looks like in practice: fewer avoidable back-and-forth cycles with fabricators/assemblers and a more predictable path through NPI.
Most late ECOs come from misalignment across stakeholders: mechanical fit issues, changing requirements, unclear ownership of revisions, or “which BOM is current?” confusion. Xpedition supports ECAD/MCAD co-design workflows so ECAD and MCAD teams can stay in sync without forcing either side to abandon their tool of choice. And with PLM-connected release discipline, teams can strengthen revision control, traceability, and lifecycle visibility – so changes are governed, auditable, and easier to communicate.
What this looks like in practice: fewer late mechanical surprises, cleaner releases, and less time lost to version reconciliation.
Supply chain volatility turns part selection into an engineering decision with schedule and revenue impact. If BOM validation happens late, it creates loopbacks that can take days or weeks, especially when alternates require footprint/model changes. Xpedition supports bringing component sourcing intelligence and BOM visibility forward so engineers can consider availability, alternates, and risk earlier, while the design still has room to adapt.
What this looks like in practice: fewer “scramble” substitutions late in the cycle and fewer redesigns triggered by parts that go obsolete or unavailable.
Engineers don’t need flashy AI—they need fewer clicks, less searching, fewer repetitive steps, and better consistency. Xpedition’s approach to AI is productivity-first: practical automation that helps users execute common workflows faster and with fewer mistakes. For example, Xpedition’s “command prediction” learns from executed commands to recommend likely next actions, reducing time spent hunting through menus, and it’s user-controllable (you can turn recommendations off). Siemens’ broader AI-enabled and algorithmic automation direction for PCB and systems design follows the same principle: intelligent automation that’s embedded into day-to-day work to increase throughput and reduce friction.
What this looks like in practice: measurable time savings across layout execution, checking, and release activities – without asking teams to “trust a black box.”
Tool churn is expensive: retraining, data migration, broken libraries, and disrupted processes can cost more than the license savings that triggered the switch. Xpedition is intentionally a family, letting teams start with what they need today and scale as complexity grows, without abandoning their workflow or design investment. Whether you begin at an entry point or standardize across a growing team, the goal is continuity: the same underlying technology foundation, with additional capability and governance as needed.
What this looks like in practice: a smoother scale-up path, less disruption, and a platform that supports you as designs move from “simple board” to multi-domain, multi-stakeholder product development.
Explore where to purchase and how to set up Xpedition products
You can buy Xpedition products directly from the product pages (PADS Pro Essentials, Xpedition Standard, Xpedtion Advanced, and Xpedition Advanced DS) or contact our sales team (Xpedition Standard, Xpedition Advanced, Xpedition Advanced DS and Xpedition Enterprise). The Xpedition product solutions are listed below, and you can explore all available options on the product pages.
Purchase PADS Pro Essentials, Xpedition Standard, along with flexible expansion options (a 25-pack or 50-pack of token), and Xpedition Advanced and Xpedition Advanced DS directly from our website.