Supply Chain Finance
The Supply Chain Finance Program uses a technology platform that links Siemens and its suppliers and subcontractors with a third-party financier (Orbian) to provide cost-effective receivables financing to those suppliers and subcontractors. The Siemens North America Supply Chain Finance program is available to suppliers providing goods and/or services to Siemens with a minimum annual value of $20,000.
SCF process at a glance
The Siemens Supply Chain Finance Program enables Siemens suppliers to improve their liquidity through the sale of their Siemens receivables to Orbian at attractive rates. A successful SCF Program is based on the collaboration between multiple stakeholders as displayed in the infographic.

Learning about Supply Chain Finance
Below are training materials that have been developed.
Payment process
Frequently asked questions:
Do I have to change the way I invoice today?
No. The existing process that a supplier performs to invoice the buyer remains in place.
Once enrolled, will all invoices be paid through the program?
For all those Siemens Buyers offering the program to their suppliers, once enrolled, all the existing and new invoices will be available for early payment. The program provides the flexibility for suppliers to request early payment for all invoices (Automatic Discounting option) or manually select individual invoices (Manual Discounting option).
How do I get paid?
The funds will be electronically transferred into the supplier’s bank account that is listed in the program’s enrollment documentation.
When do I get paid?
If the supplier is enrolled with the Automatic Discounting option, once an invoice is approved for payment within Siemens, the payment will be made in 2 business days. If the supplier is enrolled with the Manual Discounting option, once an invoice is approved for payment within Siemens, the payment will be made 2 business days after an invoice(s) is selected for early payment.
Pre-enrollment
Frequently asked questions:
What is the cost of this program?
The only cost of the program is the "discount charge" that a supplier pays to receive early payment. There are no fees to join, maintain, or exit the program.
Can suppliers enroll if their account receivables are currently pledged as collateral in a loan?
Yes. In addition to completing the standard enrollment documentation, suppliers will be provided a "Consent Agreement" that will need to be completed by their bank, allowing them to participate.
Post-enrollment
Frequently asked questions:
Once enrolled, who should the supplier contact if certain invoice(s) are not visible in the program?
The supplier should visit the Siemens IOL Portal and submit an inquiry for the invoice(s) in question. This is the most effective method to enable the Siemens AP department to research the inquiry, and they will be notified when a resolution is reached or when further information is required.
Once enrolled, can a supplier decide not to participate in the program?
Yes. The supplier is not obligated to stay in the program for any fixed period. A 30-day written notice must be submitted by the supplier to Orbian, after which the supplier will be removed from the program.