Skip to main content

Gasum Götene biogas plant

Stability and data-driven control lay the foundation for the energy systems of the future.

Biogas is increasingly highlighted as a key factor in the transition to a fossil-free energy system. In Götene, Gasum operates one of Sweden's largest and most advanced biogas projects – an initiative that not only creates local climate benefits but also serves as a powerful example of how digitalization, automation, and circular resources can drive the entire industry forward.

A Step Towards Fossil Freedom

Gasum's newly opened large-scale facility in Götene annually produces 120 GWh of liquid biogas, making it one of Sweden's largest of its kind. The plant is based on a circular system where 400,000 tons of manure and agricultural waste from nearby farms are converted into renewable energy and biofertilizer, which is then returned to agriculture. This not only means reduced emissions for transport and industrial customers – over 30,000 tons of carbon dioxide annually – but also significant environmental benefits in agriculture, where the biofertilizer improves the efficiency of plant nutrients.

Long-Term Vision and Strategic Choices

From the very beginning, the path to building a state-of-the-art biogas plant has focused heavily on digitalization and automation, which has been central throughout the entire process. With the right digital tools, facilities like Götene can not only maximize their production but also create a flexible foundation for future expansion and technological development.

Siemens control systems make it possible to connect the entire production process – from raw material flows to gas exchange and energy distribution – ensuring high operational reliability, resource efficiency, and minimized disruptions. With AFRY's Real Digital Twin, the plant could also be tested and its functionality and quality verified even before it was commissioned. This creates high delivery precision and efficient commissioning, while reducing the need for on-site work.

''We use Siemens control systems in all our facilities and are very satisfied with both functionality and reliability. The system offers good opportunities to replace and upgrade units as needed, even when components are phased out.

The modern tools, such as TIA Selection Tool and TIA Portal, provide an efficient and coherent workflow throughout the entire process – from electrical design to PLC programming, verification, and commissioning. To identify and rectify bugs at an early stage, we used a digital twin based on SIMIT, which contributed to a smoother and more efficient on-site commissioning. We feel great confidence in the control system as a long-term solution that meets both today's and tomorrow's needs. It is stable, user-friendly, and complemented by powerful tools for process visualization in the Simatic WinCC SCADA system." says Rikard Norman, Control System Specialist at Gasum.

Visual Siemens Gasum Web img 1 Web img 2 640x360

Rikard Norman, Control system specialist at Gasum

Accelerated Energy Transition

Götene clearly demonstrates that industrial, sustainable, and circular energy production is fully feasible on a large scale, where collaboration and digitalization are fundamental success factors. Biogas is important for Sweden in the energy transition because it relies on domestic resources and reduces dependence on imported fossil fuels. This strengthens the trade balance, makes the economy more resilient, and creates new jobs, especially in rural areas.

Siemens technology offers advanced digital tools that streamline the development process and optimize performance, ultimately accelerating the transition to a fossil-free energy system. The solutions are based on proven technology that can be specifically adapted for all types of energy-intensive green processes.

"At Siemens, we see it as a great privilege and fully in line with our goals to support projects that truly drive the energy transition forward. Together with dedicated energy experts like Gasum and competent partners like AFRY, we can build solutions that make a real difference. In this project, Gasum has made wise decisions to equip its facility for the future. We hope that the industry will receive the necessary political conditions going forward, including for P2X solutions, so that more projects in fossil-free fuel production can be realized," says Sofia Erinder, Vertical Owner at Siemens.

2026 februari

Visual Siemens Gasum Web img 2 640x360

Sofia Erinder, Vertical Owner at Siemens