Skip to main content
This page is displayed using automated translation. View in US English instead?

Sustainable Siemens Repair Center Stuttgart

The maintenance and repair of industrial electrical systems is the core competence of the Siemens Repair Center in Stuttgart. Around 30 employees work in the hall, which is now operated in a CO₂-neutral manner on an area of around 2,000 square metres.

Renewable instead of fossil energy

At the Stuttgart Repair Center, around 30 employees maintain and repair industrial electric motors in a hall that was getting on in years. Now it was necessary to find a future-proof solution for the approximately 2,000-square-meter hall that would contribute to Siemens AG's decarbonization strategy. An oil heating system is to be decommissioned and the energy is to be generated as sustainably as possible in the future. The goals are a CO2-neutral site with more efficient energy use and more user comfort. What was needed was a solution that was as well thought-out as it was holistic from a single source: from Siemens. The decarbonisation solution is to be implemented during ongoing operations and at the same time as the renovation of the flat roof.

Comprehensive package of measures

A concept was created for the operation of the hall that completely redefines energy generation and use. A photovoltaic system with an output of 87.4 kWp was installed on the roof – matched to its load-bearing capacity and condition. 40 percent of the annual

electricity demand is covered by the PV system alone, 73 percent of the electricity generated is used for self-use. For the heating of the hall, two air heat pumps replaced the old oil boiler. The two pumps together produce 100 kW. The primary system has an output of 85 kW, another with 25 kW absorbs heat or cooling load peaks.

Siemens-Repair-Center-Stuttgart-Halle-DJI-0970.

The basis of any efficient energy management is data transparency and needs-based control of energy systems. The Desigo CC building management system with the Desigo PX automation modules is used for this purpose. To optimise the indoor climate and further increase efficiency, radiant ceiling panels were installed to distribute the heat in the hall. They provide better radiant heat and have a cooling effect in summer. A new lighting concept further increases user comfort. With sophisticated LED lighting, pleasant light is generated where it is needed and energy consumption is reduced at the same time. Thanks to the close cooperation with the Repair Center, the retrofitting ran parallel to the roof renovation without unnecessarily affecting operations.

Transition to a CO2-neutral building

The holistic concept is paying off for Siemens' repair center in Stuttgart: around 76,000 euros in energy costs are saved year after year. The site will be operated in a CO2-neutral manner. A large part of the electricity requirement is supplied by the company's own photovoltaic system, the rest is purchased as green electricity from sustainable energy sources. With the Desigo CC building management system, the hall is optimally controlled, and the consumption data is transparent. Continuous data monitoring enables efficient system operation and makes the best possible use of the electricity from the photovoltaic system. At the same time, the holistic solution increases comfort for employees: the indoor climate is improved thanks to the radiant ceiling panels, LED lighting brings more light quality and reduces costs. The repair center is thus positioned for the future and fits perfectly into Siemens' decarbonization strategy.

Kostensenkung-2-Availability.png

76,000 euros

Less energy costs per year

Icon-Solar-pos-rgb-boldgreen.png

88,000 kWh

generated by its own photovoltaic system

Dekarbonisierung-Availability.png

NetZero

thanks to a holistic package of measures