Skip to main content
This page is displayed using automated translation. View in English instead?

Spiromatic reuses lost dough with smart rework system

Spiromatic’s smart rework system makes lost dough reusable. The result: 30% less raw material waste.

In dough factories and industrial bakeries, dough loss is a persistent reality. Recovering that lost dough was difficult until recently, as dough quickly becomes unusable. Spiromatic developed a fully automated plant that keeps the dough usable for up to 48 hours and reuses it in a controlled way in the production process.

Up to 30% loss

Pizza (dough) manufacturers punch their round pizza bases from rectangular sheets of dough. In the process, most of the corners and edges are lost. “Up to 30% of dough ends up in the waste or in pet food,” says Roel Molenaers, commercial director of Spiromatic. “Reusing the dough is not workable because it starts to rise in no time and once that happens, it is no longer reusable.”

Partly because of rising grain prices, more and more of Spiromatic’s customers were asking for a solution to that loss. “Traditionally, we have grown in transporting solids like sugar and flour. In recent years, we have been working more and more with liquids: water, oil, etc. So we built a lot of expertise in liquid handling. We started looking in that direction: liquefying the dough to reuse it.”

After two years, Spiromatic’s rework plant was ready: excess dough is misted into a tank with a rotating blade. “The knife cuts the fibres, the water irrigates the dough. So we get a new semi-finished product, which we store in a refrigerated tank. There, it remains usable for 48 hours.”

BAC Spiromatic - quote Roel Molenaers

About Spiromatic

Spiromatic develops automated systems for storing, dosing and transporting solid and liquid ingredients in the bakery sector. Solutions range from large bulk silos to micro-dosing additives.

Once dough starts to rise, it is no longer reusable.
Roel Molenaers, commercial director, Spiromatic

Every recipe is a new challenge

“A first challenge was cooling,” says Tom Windels, automation expert at Spiromatic. “Dough is a living product. And you want to pause that life. You must not cool too quickly or it will stop living. If you cool too slowly, it will still start to rise. And if you cool unevenly, your dough will partially rise. Fortunately, we already had a lot of experience in cooling liquids in heat exchangers.”

The second and biggest challenge was adding the semi-finished product again. “That’s not just a matter of pumping through. How much rework we add is different for each customer and even for each recipe. Nothing must change about the final product: taste, colour and other properties must remain absolutely the same. So we have to start determining how much rework each recipe can ‘tolerate’ based on customer testing. For that, we designed a mobile installation.”

“Scalability was also a hard nut to crack. At the lab scale, a process behaves differently than in an industrial context. There is quite a lot of complexity in the line, but it worked: the only limiting factor left is the size of the client’s building. As long as he can use all the rework within 48 hours, there is no limit to the size of our process.”

BAC Spiromatic Tom Windels
The balance between fresh dough and rework is crucial. Automating that while keeping your final product perfect was the biggest challenge.
Tom Windels, Automation Expert, Spiromatic

Smart control with PID Control

The heart of the system is a rugged PLC: the redundant SIMATIC S7-1516. “For small test rigs, smaller PLCs are sufficient. On large integrated projects, we used to use multiple PLCs to communicate with each other. That created a lot of overhead, making the whole thing increasingly complex. Siemens advised us to house the whole thing in one PLC and keep it redundant. It works perfectly that way.”

Spiromatics installation demands quite a lot from the PLC. “We constantly monitor quality with temperature sensors and viscosity measurements. It includes volumetric and mass flow meters, SIWAREX weighing modules, etc. The PLC processes all that data and automatically adjusts the process based on PID Control, a technology object in TIA Portal. That made integration a lot easier.”

“The PLC has to coordinate three processes simultaneously: creating the rework, controlled addition and cleaning the plant completely,” says Ludo Dejaeghere, CEO at Spiromatic. “Some customers run full-time, so then we have to clean parts of the plant while it continues to produce. Obviously, no cleaning agent should enter the production. That flexibility and modularity require a lot of computing power.”

BAC Spiromatic - PID Control

The ultimate optimisation

The rework plant has been on the market for a year. More and more manufacturers are now avoiding up to 30% food waste. This reduces their raw material costs, but also CO₂ emissions in raw material production, transport and waste disposal. “For me, Spiromatic sets a new standard in the bakery world with this,” says Thomas Vermeir, account manager at Siemens. “What producer can still do without it? We are very proud to have collaborated on such a ground-breaking innovation.”

BAC Spiromatic - Thomas Vermeir
For me, Spiromatic sets a new standard in the bakery world with this. What manufacturer can still do without it?
Thomas Vermeir, Account Manager, Siemens

“We have been an OEM partner of Siemens for six years,” Ludo adds. “We are getting a lot of support and it has definitely helped to bring this project to fruition. It is also in this way that we like to work with our customers: in a partnership, where we look for solutions together. They have an enormously wide range of technology, but they still manage to be highly responsive. This is important because we also provide 24/7 support to our customers.”

The rework plant has already found its way to processors of pizza and pastries. There are many manufacturers on the market that are not yet using raw materials optimally. Yet Spiromatic is already working on its next project: reuse of baked goods. “It is still in its infancy, but eventually we also want to be able to reuse all baked products that do not meet the standard for whatever reason. That will reduce food waste much further.”

Thanks to Siemens’ in-depth support and continuous availability, we have brought this project to a successful conclusion.
Ludo Dejaeghere, CEO, Spiromatic

The benefits in a nutshell

  • Up to 30% less lost dough
  • Lower raw material costs through re-use of ingredients
  • Energy and CO₂ savings thanks to less transport and waste disposal
  • Constant product quality thanks to precise process control
  • Higher uptime: system continues to run in parallel during cleaning

Curious about the possibilities of TIA Portal?

Discover them here.