Inspekto is delivered with everything you need – it contains a Siemens Industrial PC, a camera, a light and all the required cables. That means there are no extra orders to place, no looking around to see if you have the right connectors. Where to install it? That’s totally open too, because the solution has been conceived for a variety of use cases – from production lines to robots. Multi-camera setups are also possible, for example in complex production cells where several inspections are done at the same time. Inspekto can be fully integrated with PLC or MES/ERP systems, which makes it great for the inspection of incoming goods or the final quality inspection of finished products.
Once you have decided on the use case and the hardware is in place, AI guides you through the training process. The initial step is training the model using a dataset of just 20 good samples, focusing on factors such as quality, form and accurate labelling. Bad samples are optional, not mandatory. Users get instructions via the Inspekto software for every step of the journey. There’s no guesswork, as it tells users which data to add and when. All in all, it usually takes less than a day to get everything going. These time savings are down to the fact that this is not a traditional machine vision solution requiring extensive customisation by experts for each use case.