Manifold challenges
The production system is controlled by a central programmable Simatic S7-1500, and each robot cell also has its own control system. Thanks to stored recipes, the controls ensure, for example, that the right process runs for each of the various packaging formats and that the robot cells always receive supplies of trays and cheese. No other system at Emmi is so complex, reveals Purtschert: "The cutting process for the delicate cheese pieces is very demanding, and the cheese is of different hardness depending on temperature or degree of ripeness. In addition, the shape of the pieces must be right, the robot must not compress them and must arrange them perfectly in the packaging." Since the cross-shaped gripper constantly rotates around its own axis, Robofact had to arrange the cable routing so that no cable can get caught.