Skip to main content
This page is displayed using automated translation. View in US English instead?

Motion control helps handle complexity with ease

Max Schlatterer GmbH & Co. KG wanted everything under control: The complete control, robotics, safety and operation of an ultra-compact cross-milling system runs with Efficient Motion Control Solutions for Industry to create an extremely flexible solution that’s exceptionally easy to use.

Compact, flexible, and easy to use with motion control

The goal was to be able to process the most demanding tasks with a wide variety of pitch and tilt angles and to achieve perfect quality with a minimum footprint — and project manager Oleg Akst and the team at Max Schlatterer GmbH & Co. KG rose to the task. They automated a new cross-milling system for conveyor and drive belts with a comprehensive, completely integrated automation and drive solution that enables them to configure and engineer all operations in a uniform, easy-to-use environment. This way, they save both time and costs in engineering and could design a processing solution that’s exceptionally compact and flexible.

Reference Max Schlatterer Gmbh & Co. KG Esband

Key benefits

50 % less time to be operation-ready

Benefits for engineering and commissioning: Compared with mixed systems, the uniform motion control solution and the integrated validation cut the time required for commissioning in half.

30 % less effort for documentation

Benefits for approval and safety: The precertified system components and safety communication streamline the safety acceptance process.

80 % less training required

Benefits for operation and scale-up: The standardized HMI design and easy parameterization using G-code reduce the training requirements for future projects by a large margin.

An employee shows a variety of conveyor and drive belts to another man

Greater flexibility for complex processes

Whether transporting sausage products, manufacturing paper straws or dispensing bank notes at ATMs, “Esband” endless conveyor belts from Max Schlatterer GmbH & Co. KG have built a reputation for exceptional quality, durability and resilience. The company develops most of the highly specialized production solutions for these belts in-house, including a new machining center for belt manufacturing: A six-axis machining system with an articulated-arm robot mills belts with various angles and geometries. What’s more, all machine operations and movements are controlled by a single SIMATIC Technology CPU — including the robot, controlled directly via the SIMATIC S7-1500 T-CPU.

One-for-all solution: Motion control, safety, robotics

For the milling system, Oleg Akst and his team relied on a solution they had previously implemented in another processing unit: A gantry system for strip processing had recently been automated using a SIMATIC S7-1500 T-CPU. Although the robot’s six-axis kinematics made the motion control application for the cross-milling machine significantly more complex, “we were still able to leverage a great deal of our existing expertise,” says Akst. He and his team can engineer all components in TIA Portal: “SIMATIC T-CPU, SINAMICS servo drives and the SIMOTICS servomotors — motion control, robotics and safety are all implemented in a single project.”

Photo of the main SIMATIC Technology CPU that also controls the milling robot.
View inside a control cabinet

Integration delivers benefits over the entire life cycle

Harald Bischoff, head of engineering at Max Schlatterer GmbH & Co. KG, was also immediately enthusiastic about the idea of integrating the robot into the automation system as a purely mechanical component: “A single CPU in the system that controls the machine and robot, using standard components and without any additional hardware, offers enormous advantages for engineering and operations. We can test the entire automation system with a single tool, which makes it very easy for our teams to validate the project and saves time during commissioning and, of course, later on when it comes to issues like service or upgrades.”

Integration also accelerates engineering

Oleg Akst explains how the engineering process benefits from the unified and integrated motion control solution: “With SIMATIC Safe Kinematics, we can visualize the movements of the system and the robot in the engineering environment already during development and design. Especially with such a compact system, this ability gives you tremendous confidence that everything will work just like it should. After all, we have to account for all machine parts: the robot with its 6D kinematics, clamping axes and drive rollers. All units have to be coordinated. Thanks to the integrated tools, we can also prepare for commissioning much more effectively. Overall, this solution saves us at least half the time compared with solutions with additional interfaces.”

Employee accessing TIA portal on a laptop
A laptop with the G-Code Editor on the screen

Flexible adjustments during operation via G-code

The result: “After just two days, the system was ready for operation, the operators had been trained and we were able to start production. It was really great to see how quickly our people got the hang of it.” All machining parameters can be adjusted during operation directly via the integrated G-code Editor: “This operator can modify the program during operation without needing an engineering tool or the engineering department.” And because the HMI and operation are structured the same way on all other systems similar to this one, training is almost entirely eliminated when implementing new projects, adds Bischoff: “When we implement additional projects and machines with the Siemens solution in the future, we can reduce staff training costs by up to 80%.”

A flexible safety solution builds trust in technology

Thanks to the sophisticated safety solution, the operator can even load the machine while the robot is still in operation. The robot’s work area is divided into two independent zones both physically and through a matching safety logic. Each zone is monitored separately to ensure that program changes do not compromise safety zones and do not result in unintended collisions, as Akst illustrates: “This makes operators feel perfectly safe when working with the system, because no matter how, for example, the movement of the tool on the robot is changed, the entire arm is always monitored.”

Control panel on a machine
Screenshot of precertified building blocks in the files explorer

Less effort for safety acceptance test and documentation

The safety building blocks and components, as well as safe communication via PROFIsafe, are delivered with the required certification, Akst continues: “This precertification streamlines safety acceptance testing and documentation, allowing us to shorten the safety acceptance process by roughly 30%.” As a result, Max Schlatterer GmbH & Co. KG is all set for the machine safety requirements for the EU Machinery Regulation, the expert adds: “I don’t see any issues there with respect to CE marking.”

Usability is key

For Bischoff, however, another aspect is equally important: “We need qualified operators for our manufacturing processes. That’s why we wanted to leverage existing know-how — for example, by letting operators adjust programs directly via G-code, a standard language widely known and used in machining and mechatronics.” Operating the robot is now just as easy as operating any other type of machine that Max Schlatterer uses for production, and Akst has already noticed how this changes the mindset on the shopfloor: “We’re already getting inquiries from production asking if we can implement even more processes with the robotic system, simply because the system is so flexible and easy to use. And the best part is, the answer is often ‘sure,’ because the machine operators can change and program so much so easily by themselves.”

An employee operating a machine via the HMI panel
“With the new machine, we can implement new requirements via G-Code without software development having to engineer new features. That’s just great.”
Oleg Akst, Project Manager, Max Schlatterer GmbH & Co. KG
SIMATIC Motion Editor

From motion code to robot execution

The story of Max Schlatterer GmbH highlights the significance of usability and flexibility in robotics. With the SIMATIC Motion Editor tool, we support users in creating, validating and transferring robot path programs with features such as file inspection, syntax check and path preview.