Gregory Conte is Inventor of the Year 2024: His invention makes smart buildings even smarter.
'Smart buildings can have thousands of data points, sensors and actuators such as thermometers and hygrometers, dampers and valves,' Gregory explains. 'To analyse a system, we need as much information as possible about these data points. For example, a thermometer can measure the indoor or outdoor temperature of air, water and so on. There are labels or tags that are associated with each data point. In general, all the information we need to label data points for analysis is available somewhere in the customer’s data. However, customers use different BMS vendors and have highly variable naming conventions, so there’s no universal direct mapping to the tags, which we need for our analytics tools. Therefore, the onboarding process, especially the correct labelling of data points, has been a tedious manual task.'