Skip to main content
Exterior view of the University of Toronto Scarborough Campus (UTSC). (UUID:64470b97-7e85-4e28-84a4-39b396196eae)

Decarbonizing campus with simple high-impact strategies

The University of Toronto Scarborough Campus (UTSC) in Canada advances sustainability and targets carbon neutrality by 2050. A recent project in Environmental Science and Chemistry Building shows how simple efficiency upgrades can drive major decarbonization and create savings on campus operations.

Small change, big difference

The LEED Gold-certified Environmental Science and Chemistry Building (ESCB) at UTSC houses the Department of Physical and Environmental Science and serves over 1,100 undergraduates and 150 graduate students. Inefficiencies in the heat recovery chiller of its geo-exchange system led to unexpectedly high natural gas consumption during colder months, challenging UTSC’s decarbonization goals.

Interior view of the University of Toronto Scarborough Campus (UTSC)

33% Less natural gas consumption

As a result of fuel switching, a significant decrease of 33% in natural gas consumption was observed.

4% Reduction in electricity usage

Through the systematic recommissioning process and the utilization of advanced control strategies, a reduction of 4% in electricity consumption was achieved.

1,094t Annual GHG savings

Making existing equipment operate as efficiently as possible is the ideal starting point for a decarbonization journey. Optimizing existing infrastructure alone has yielded a greenhouse gas emissions reduction of 1,094 t CO2e.

Efficiency optimization of the geo-exchange system

Mechanical room in the UTSC basement featuring insulated pipes, pumps, and energy‑efficient building systems used for campus heating and cooling infrastructure. (uuid:7edcb64a-33a9-4ecb-883e-5d1139fce85a)

Performance improvments without disrupting daily operations

The ESCB was designed for energy efficiency and equipped with a geo-exchange system. However, the heat recovery chiller wasn’t working as intended, which had a cascading effect on the entire system’s performance. The University of Toronto Scarborough Campus also faced the challenge of recommissioning the building while it remained in use. Through Existing Building Commissioning (EBCx), UTSC identified and resolved inefficiencies, improving the performance of legacy systems and infrastructure without disrupting comfort and daily operations for students, faculty, and staff.

The Siemens team wasn't just interested in fixing things – they wanted to help us build something sustainable for the long term.
Johnny Ravindran, Manager of Energy Management and Implementation, UTSC

Advancing the campus for tomorrow

UTSC partnered with Siemens to optimize the ESCB with support from the IESO SaveOnEnergy program and Enbridge Gas. This collaborative approach to Existing Building Commissioning (EBCx) leveraged data‑driven problem‑solving and provincial resources and incentives to reduce energy consumption.

Johnny Ravindran, Manager of Energy Management and Implementation is standing on the roof of the UTSC in front of the roof fans that support the building technology or HVAC system. (uuid:9ab605bc-86c0-4f91-b12f-6b2b714dbfd8)

System review and design verification

The optimization process began with a comprehensive system review. Siemens experts analyzed system data and collaborated with the UTSC team to assess the building’s energy loads and their integration with the existing geo-exchange system. The heating and cooling loops were carefully evaluated, and the original design specifications were revisited to identify deviations from the original design and inefficiencies.

Functional testing and control system tuning

In the next phase, functional tests were carried out to ensure all systems were operating as intended. This included verifying the responsiveness of the control systems and fine-tuning the PID loops to achieve more accurate and stable control of heating and cooling functions.

A functional testing and control system tuning showing a temperature and pressure gauge. (uuid:cb9720d6-79c2-4579-a6d1-925d979a68ed)
Mechanical room in the UTSC basement with labeled geothermal and chilled water pipes, valves, and control units supporting the building’s HVAC system. (uuid:9fb35ded-7f79-4f17-b18f-8c0e32b0b22b)

Performance measurement and heat monitoring

A BTU meter, a device tailored for accurately measuring thermal energy exchange in heating and cooling systems, was installed to monitor the heat produced by the heat recovery process. This allowed for accurate measurement of supply and return line flow rates and temperatures, providing valuable insights into how effectively energy was being captured and reused within the system.

Optimization and implementation of corrective measures

Finally, the geo-exchange system was fine-tuned according to recommendations from the commissioning study to enhance overall efficiency and performance. Additional improvements were implemented across the building’s HVAC systems, including HVAC scheduling, chilled water optimization, hot water loop tuning, air-handling unit setpoint adjustments, and earth tube optimization.

Johnny Ravindran stands in front of a control unit supporting the building’s HVAC system in the UTSC basement. (uuid:fecb070e-c815-4613-b87a-23ed42557a49)
Optimizing the way the building runs is a key thing we can do with great payback.
Patricia Escobar, Sustainability Manager, UTSC

Let’s decarbonize your existing building together

Eine Gruppe von Studierenden läuft gemeinsam und lächelt.

The successful EBCx project at UTSC demonstrates how targeted, cost-efficient measures can significantly improve the energy efficiency and sustainability of a university building in a short time. Are you also looking to make your existing buildings more sustainable? Get in touch with us! Together, we’ll identify the right approaches and develop an effective strategy.