The core of this teaching material is based on Teaching Theory 3.0. Each chapter is an independent learning unit. Each chapter always focuses on its specific objective. After downloading the textbook, detailed explanations of relevant theories will be provided in the chapters. For each chapter, a specific task will be set, and then this as an example template will be used to formulate plans and implement them specifically. Finally, when completed, a checklist will be used to test the execution status according to the structured step-by-step guidance. After that, there are exercises where students independently complete the planning and implementation. The final checklist is helpful for self-checking the answers.
What is Industry 4.0
Industry 4.0 is a high-tech strategic plan proposed by the German government. The project is jointly funded by the German Federal Ministry of Education and Research and the Federal Ministry of Economic Affairs and Technology.