Plant by plant, step by step migration
“Connecting the local control systems to the central control system was quite a challenge,” says Andre Albers, Siemens Digital Industries sales representative. EGLV and Siemens found an innovative, reliable, cost-effective, and secure solution that used existing public networks and a VPN tunnel. The first plants were successfully migrated. Close collaboration between the local staff and the project team helped facilitate the adoption of the new system. To reduce cost, EGLV integrates each plant into the system one-by-one when the local process control solution is due for an upgrade. Next in line are large wastewater processing plants serving the equivalent of more than half a million people.
Flagship projects
In addition to upgrading existing plants, EGLV completed the construction of the new Emscher sewer running between the Dortmund-Deusen and the Emschermündung wastewater treatment plants. The 51 km long sewer collects wastewater of over 2,26 million inhabitants, as well as large volumes from industry and business, and routes them to the Bottrop and Emschermündung treatment plants. One of the sewer’s three large pumping stations and the new solar-thermal sewage sludge drying plant run on the virtual platform. Both applications were flagship projects within the region and for EGLV.
Revitalizing the environment
“As part of the digital transformation at EGLV, we are particularly interested in further utilizing our plant data by creating digital twins and the use of artificial intelligence in plant operation.
This digitization project is not just an end in itself, it also has a higher value. Our goal is to create livable spaces for people and nature along the Emscher and Lippe rivers.” Dr. Emanuel Grün explained at the time.
By betting on the right technologies to improve its operations, EGLV ensured that the 30-year Emscher renaturation project held its course and that residents, animals and plants can enjoy a safe and natural habitat for many more decades to come.
November 2022