Skip to main content

Цифровізація унікального джерела білка

Технологія Digital Twin від Siemens дозволила Nasekomo створити франшизу з вирощування комах, орієнтовану на постачання високоякісних кормів для тварин.

Insects are delicacy for many animals: chickens and pigs root them out of the soil, fish leap from the water to catch them, and even dogs enjoy chasing and snapping at them. Nasekomo, a company based in Bulgaria, has created a franchise model for farming insects for animal feed. Digital Twin technology from Siemens has been essential for standardizing operations and for helping the company live up to its sustainability goals; Siemens Xcelerator provides a competitive advantage by accelerating digital transformation.

Scientists estimate that there are between 2 million and 30 million insect species worldwide, yet only 900,000 of them have been described. At Nasekomo, though, attention is centered on just one species: Hermetia illucens, commonly referred to as the black soldier fly.Insects are one of the most sustainable animal protein sources, and the demand for sustainably produced, insect-based protein, oil, and frass (a valuable fertilizer) is expected to grow significantly. As a pioneer in industrial-scale insect-based bioconversion, Nasekomo seeks to serve the market by providing technology and know-how to its future franchise partners.

A robotic arm is assembling a component in an industrial setting.

Beginning as a demonstration center

A vertical farming app interface showing a plant growth simulation with various settings and options.

The company started with an industrial demonstration center near Sofia, Bulgaria, with a focus on the larvae phase of the black soldier fly lifecycle. The larvae are fed a diet of organic byproducts from agriculture and beverage production, such as beer. In ten to twelve days after hatching, they reach their optimal size and weight for processing. At that point, the larvae are blanched. What follows is a process to create protein meal and insect oil. The frass and leftovers from the process are prepared as fertilizer. Altogether, Naskomo’s process exemplifies a circular economy model: it produces animal feed from organic waste using bioconverting insects, and what is left over from the process serves as a fertilizer.Nasekomo’s approach is to scale up operations under an AI-driven franchise business model. In 2025, the construction works of its first franchised factory will start, also in Bulgaria.The company offers a complete franchise package, including technology, feed preparation methods, and black soldier fly newborn larvae from its MultiFly center, which is part of the demonstration center. Notably, these larvae benefit from genetic advancements developed at the adjacent Fly Genetics program.“We’re aiming for exponential growth to meet the demand for 2.5 million tons of protein per year by 2030. Franchising is our key strategy to accelerate our expansion,” says Marc Bolard, co-founder and CEO of Nasekomo. Using a creative future-digital platform from Siemens, Nasekomo will be capable of supporting more than 100 production sites.

Standardization as the basis

Every businessperson will attest that standardization is the cornerstone of a thriving franchise – and all the more for companies in the future-food segment who want to scale up economically. Nasekomo has partnered with Siemens to lay the groundwork for standardization. The alliance was kicked off over two years ago with a series of workshops. Nasekomo’s people contributed their extensive biological knowledge of the black soldier fly, particularly their understanding of the larvae phase in a controlled environment. Siemens brought in their experts for process industry, IT/OT convergence, data security, cybersecurity, and food and beverage. “By assembling these diverse teams, we were able to come up with an actionable digitalization strategy,” says Rok Koren, Senior Digitalization Advisor at Siemens Slovenia.For Nasekomo co-founder and co-CEO Marc Bolard, one thing stood out at the beginning of the partnership: “Soon after we started collaborating with Siemens, we quickly understood the need for proper simulation.” And that means one thing: a Digital Twin. Siemens’ experts went to work on creating a Digital Twin of production using Tecnomatix Plant Simulation software. The first digital twin was of the Nasekomo demonstration plant, and for each subsequent plant a Digital Twin will be created as a matter of course. The idea of standardization also extends to choosing the same technology from Siemens for all sites, such as Simatic WinCC Open Architecture for the SCADA system, and a common approach for the convergence of IT and OT. This high level of digitalization enables access to open and interoperable digital tools and solutions created with partners in the Siemens ecosystem and available at the Siemens Xcelerator Marketplace.

A digital twin visualization showing interconnected systems and data flow in a technological environment.

Designing every detail, managing the bigger picture

A visual representation of sustainable industries with a focus on green technology and eco-friendly practices.

But the whole journey with Siemens doesn’t end with the design and the simulation of the entire plant, it also includes the design and data management of every single component and machine in it. That’s why Nasekomo trusts the Siemens Xcelerator Software portfolio, namely Solid Edge and NX for design and Tecnomatix Plant Simulation for production process improvement.Solid Edge and NX, both part of the Designcenter suite, enable faster design iteration, allowing quick modifications and rapid prototyping. “Stability is important when it comes to saving time and avoiding data loss – and Solid Edge is very stable,” Bolard remarks. “Furthermore, it integrates with our PDM system for efficient data management and version control. Additionally, its precise drafting tools help engineers create detailed 2D drawings and annotations with accuracy.

A better energy balance

The Digital Twin data from Nasekomo’s franchisees will be relayed to operators at the company’s headquarters in Bulgaria. From there, they will monitor operations and provide remote support and maintenance. A robust Industrial Cybersecurity concept is in place to ensure secure communications.First and foremost, the goal is to help franchisees make their operations more sustainable. One example is to better manage and control energy flows with Simatic Energy Management Software, which can also pinpoint ways to feed excess heat back into processes. Another is to determine the product carbon footprint from production using SiGREEN, a comprehensive product carbon footprint solution for managing and reporting supply chain and production emissions.

Siemens Xcelerator logo featuring a stylized 'X' with a dynamic and forward-moving design.

Next step: going beyond insects

A promotional image for Siemens featuring a futuristic, sleek design with a prominent logo and a tagline.

Nasekomo’s current focus on building Digital Twins for insect breeding plants is just the beginning. These advanced technologies, designed to optimize processes in insect farming, hold potential for broader applications in the future. From monitoring and managing tomato cultivation to optimizing chicken farms or even controlling conditions in mushroom production, the flexibility of digital twin technology can transform various agricultural sectors. “By developing these systems today, Nasekomo is paving the way for smarter, more efficient solutions that can be adapted across the food industry”, says Marc Bolard.
November 2024
Contact: Rok Koren

What's in a name?

Nasekomo isn’t just the name of a business concentrating on insect protein, it also means “insect” in Bulgarian. The company is a collective of entrepreneurs, scientists, and engineers working toward a more sustainable future by establishing a network of factories to grow black soldier flies as a source of protein, oil, and fertilizer for the feed and agricultural industries.
Nasekomo