Пожалуйста, выберите другой браузер

Похоже, вы используете браузер, который не поддерживается. Обратите внимание: это может повлиять на отображение сайта и его юзабилити. Мы рекомендуем скачать последнюю версию браузера или установить другой.

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

продолжить в текущем браузере

Efficient on-site power supply

image

Industrial power plant solutions

Make an investment in your independence – and ensure a reliable and flexible power supply for your processes. Electricity and heating are major cost factors for industrial plants. That means there’s a long-term cost benefit in having your own power plant at your factory, mining, or production facility. It also helps you achieve climate goals and stay ahead of the competition. Siemens will create just the right power plant solution for your purposes.

Make the most of fuel - Combined Heat and Power portfolio
Download brochure
image

The future energy hub of South America

Energizing Bolivia

Power plant portfolio

Your power plant – uniquely fitted

Every industry, every factory, and every facility has its own unique demands for power supply. That’s why we configure and optimize your system individually, from the initial design to the final component. It goes without saying that we incorporate technologies proven in hundreds of facilities and over thousands of operating hours. Another factor that cuts your project risk: We pre-manufacture entire modules and test them away from the construction site. This means much less expense incurred on-site at your facility.
 
  • From power train to turnkey power plant
  • Available as a simple cycle or as a combined cycle power plant
  • With aeroderivative turbines or industrial gas turbines, depending on the power output required
  • From 14- to more than 230-MW output, for 50 Hz or 60 Hz grids

At home in industry

Siemens has a thorough understanding of the processes in your industry. After all, we’ve been building, expanding, and modernizing all kinds of industrial facilities for decades. We know that production processes have to be closely interlinked with ancillary activities like electricity and heat generation and energy distribution. Only once everything is integrated can the opportunities for automation and digitalization be exploited to the full.

image

Steel and cement

Processing mineral raw materials requires a vast amount of energy. That’s why procuring electricity and heat makes up a significant proportion of operating costs. Entities that supply their own electricity and heat using their own power plant will enjoy significant cost savings. And with a sturdy, state-of-the-art combined cycle power plant, they can also substantially improve their environmental life cycle assessment.

image

Oil and gas

From production to transportation and refining – the oil and gas business is getting tougher. Increasingly stringent environmental regulations are forcing many players to take action. Companies that invest in state-of-the-art on-site power generation enjoy multiple benefits – by curbing their emissions through the flexible use of available raw materials and also by using technologies that seamlessly integrate into their production systems. Siemens provides you with robust mechanical engineering that will operate reliably – even with frequent changes of load and fluctuating gas quality.

image

Pulp and paper (fiber industry)

Whether you process recycled fiber or use cellulose and lignin from the raw material wood, your systems will consume large volumes of electricity and heat. Generate your own process steam with an integrated power plant on-site. Siemens offers plants with combined heat and power (CHP) in all scales to meet every need. That means you can remain flexible and independent over the long run.

image

Mining

Mining is all about raw materials. When it comes to competition, it is production costs that matter – and energy costs are a key factor. The remote regions where raw materials are extracted are often not connected to public power networks. An on-site supply requires flexible facilities that can deliver power under tough conditions at low cost. Whether it’s for open-cast or underground mining, in cold or hot environments, as a standalone system or a back-up for renewable sources – Siemens will design and build exactly the power plant solution you need to bolster your competitive position.

image

Chemical

Safety is paramount in chemical processes, and outages are both risky and costly – so your electricity supply must be totally reliable. This works best if you have your own generating system on-site, which will make you independent of external suppliers and curb costs in the long term. If a power plant also permits heat extraction, all the better – that will make your entire system even more efficient. We build the right solution for you – and integrate it seamlessly into your chain of processes.

image

Utilities and independent power producers

The energy landscape is changing. Small gas-fired power plants will be a mainstay of our energy supply system for the foreseeable future. That’s because they can serve as a flexible back-up for renewables, they’re highly efficient and operate reliably, and they can enable regions to function independently. On islands or at remote industrial sites, covering basic load or peak, with or without heat extraction – an industrial power plant solution from Siemens will perfectly suit your specific requirements.

Reliable solutions – outstanding performance

image
  • Scale: from a small 4-MW solution with a single gas turbine to a multi-shaft combined cycle power plant with a power output of 230 MW or more
  • Scope: from power train to turnkey power plant with a performance guarantee
  • Efficiency: an overall efficiency of up to 90 percent can be achieved with combined heat and power (CHP)
  • Key components: highly efficient gas and steam turbines, steam generators, and instrumentation and control from Siemens
  • Benefits in operation: minimized emission and fuel costs, maintenance-friendly systems

Efficient turbines: the heart of every power plant

Downloads, support and services

Your source of information

This is where you can find material to download, contact details, and links to the services we offer.

Energy Customer Support Center

Siemens AG
Freyeslebenstrasse 1
91058 Erlangen

(Charges depending on provider)
(From the German fixed network € 0.14/min.
and from the German mobile phone networks max. € 0.42/min.)

image

Training

31 training centers worldwide – we offer customized trainings. Benefit from our network of experts.

Go to Power Academy
image

Plant service

Maintenance, repair, modernization – our Power Generation Services ensure that your facility maintains its value. Enjoy long-term confidence.

Go to Power Generation Services
image

Financing

From consulting to financing – Siemens offers financing solutions for business-to-business customers worldwide. Talk to the experts.

Go to Siemens Financial Services
image

Online customer portal

The latest information, news, product details – get information direct from Siemens in our exclusive Customer Portal. Keep your finger on the pulse.

Go to Power and Gas Customer Portal

References

Siemens power stations supply the world

More than 1,500 Siemens power stations are in use around the world. Here are some of our top projects we have implemented with our customers.

image
image

News

Media and events

The latest news about our projects. Industry events that affect us – and you – in your market. Find out what’s happening in the world of industrial energy supply.

Contact

The path to the power plant solution you need

Do you want to supply your facility with power, reliably and cost-effectively? Or free yourself from reliance on a costly public supply? Do you need a flexible reserve power plant? Together we’ll find the perfect solution for your particular challenge.

image
Talk to us about your needs
Contact