Sensformer: Transformers meet connectivity

image

Sensformer: Born connected.

Are you ready to move into the age of connective assets? With the Sensformer, a transformer that is equipped with a connectivity feature, you can utilize the data your transformer provides to dive into digitalization and optimize your operations and business decisions.

 

Discover the Sensformer and all the benefits

Can transformers only transform energy? Find out in our iPDF.
Download now
image
Power Transformers

Power Transformers

  • Rated power: from ≤ 100 MVA to > 400 MVA
  • Application areas: power generation, power transmission, industry, infrastructure
  • Features: available in special low noise version, designed to be highly efficient with “green” transformer options
image
Reactors

Reactors

  • Rated power: from ≤ 10 MVA to > 400 MVA
  • Application area: power transmission
  • Features: available in special low noise version, designed to be highly efficient with “green” transformer options
image
Transformers for Industrial Applications

Transformers for Industrial Applications

  • Rated power: from ≤ 10 MVA to > 400 MVA
  • Application area: industry
image
Phase Shifting Transformers

Phase Shifting Transformers

  • Rated power: from ≤ 10 MVA to > 400 MVA
  • Application area: power transmission, industry
  • Features: available in special low noise version, designed to be highly efficient with “green” transformer options
image
HVDC Transformers

HVDC Transformers

  • Rated power: from ≤ 10 MVA to > 400 MVA
  • Application area: power transmission
  • Features: available in special low noise version, designed to be highly efficient with “green” transformer options
image
Distribution Transformers

Distribution Transformers

  • Rated power: from 5 kVA bis ≤ 30 MVA
  • Application areas: distribution MV, industry, infrastructure
  • Features: designed to be highly efficient with “green” transformer options
image
Traction Transformers

Traction Transformers – Tractronic®

  • Rated power: ≤ 10 MVA
  • Application area: mobility
image

Success Story, июля 31, 2018

Live remote monitoring system for Factory Acceptance Tests

Don't miss our latest News
Subscribe to Transformers Newsletter

A key role in electricity supply

Current highlights

Direct-current electricity can now be transmitted at gigantic 1,100 kilovolts

The world´s first transformer, which has been designed and manufactured for the HVDC transmission line with the highest direct-current electricity of ± 1,100 kilovolt (kV) has been tested successfully in Nuremberg, Germany. The transformer will enable low-loss and extremely efficient high-voltage direct-current (HVDC) power transmission over a record distance of 3,284 kilometers with a transmission capacity of twelve gigawatts.

 

Excited? You can watch part 1 and part 2 of the entire films on Siemens’ first 1,100 kV HVDC transformer on YouTube.

Part 1

Part 2

Find out how our innovations are shaping the future of transformers

There’s so much more to a transformer than just transforming voltage: They actually form the backbone of modern energy grids, and their reliable operation is crucial to ensuring a stable and resilient power supply.

 

If you haven’t had the chance to see our transformer model in person, now you can learn all about innovative transformer technology from wherever you are by watching the playouts online.

Innovative traction transformers “Tractronic® Thinity”

image

Siemens presents its latest innovation highlight: The Tractronic® ThinityTM transformers will be installed in the trendsetting Siemens regional train platform Mireo®. The highly innovative transformer design results in an ultra-low weight of the infinity-symbol shaped Tractronic® ThinityTM transformer (approx. 25% less weight). The decreased weight will not only make the trains less energy-consuming. There will also be a higher capacity for passengers, monitoring equipment and passenger infotainment on board. Further benefits of the development are: more freedom of movement, shorter construction times, and optimized components – together these aspects form the truly unique Tractronic® ThinityTM transformer.

 

Download our Tractronic® Thinity brochure

Distribution transformers in new clothes

image

In March 2017 Siemens was honored with the IF award for its innovative transformer design. Along with the eye-catching layout of its transformers, Siemens now announces the renaming of two product lines: FITformer and GEAFOL Neo. FITformer is the name of the transformer family now congregating all liquid immersed distribution transformers while GEAFOL Neo is the modern version of the current GEAFOL Basic. The new brand names reflect Siemens’ innovation leadership and top-end quality. Siemens FITformer and GEAFOL stand for eco-friendliness, high efficiency and maximized availability. While the names and visual appearance of our products will change, our expertise and quality remains the same. 

Resilience: Pretact® – React in advance

Keeping grids resilient - at any time with Siemens Transformers

Reliability of energy grids is a matter that effects everybody involved in the business. Siemens Transformers offers a whole portfolio to offer grid resilience wherever needed. Our concept, named Pretact®, for resilient grids comprises a three-pillar-plan to enable our customers to prevent failures, protect their equipment and react in cases of emergency. Learn more on this topic in our infographics, use cases and collaterals. Our new concept addresses emergencies, retrofits and new installations along the entire energy value chain to increase network stability by modular feature/ solution architecture for power and distribution transformers.

Installing a mobile resilience unit within 3 days

The idea of mobile resilience units is to replace a large EHV-transformer by three compact and versatile single-phase units – either for planned or unplanned outages. The transport and installation can be completed within 30 working hours.

 

See in our slideshow how it works!

Visual Design: Shaping the future of transformers!

image

Have you ever asked yourself why a transformer looks the way it does? The most innovative engineering, materials and technologies are hidden inside. We have decided that in future our leading electrical and mechanical design should be visible from the outside.

 

Honored with the coveted iF Design Award 2017: the Transformer Family Design and the Design of the Mobile Resilience Unit as part of the Pretact® Concept.

Ecodesign

Check your transformer’s compliance with EU requirements

As of July 2015, distribution and power transformers put into service within the European Economic Area (EEA) must comply with the new requirements of the Ecodesign Directive from the European Commission. The directive aims to improve energy efficiency, environmental compatibility and thus to reduce CO2 emissions. Siemens transformers can be designed to fulfill the new EU requirements.

Does your transformer’s Peak Efficiency Index satisfy the new EU requirements?  

The entered values equal a Peak Efficiency Index of

%
Target value:
Your transformer satisfies the new EU requirements and is ready for action!

If you still have any doubts or questions, we are pleased to help you.

Your transformer does not satisfy the new EU requirements and is not allowed to go in operation within the EEA. The loss level has to be decreased.

We are pleased to help you with any questions or further information.

Calculate your transformer’s efficiency

With our free Siemens Transformer App, you can calculate and compare noise and efficiency values of different transformers on the fly:

Always get the most out of your products

Do you have any questions regarding our transformer services?
Contact our support

Fields of operation

Find out why Siemens makes a difference

In more than 100 countries and for more than 100 years, transformers made by Siemens have been synonymous with top quality. The extreme high reliability (mean time between failures) is only one example of this quality. To ensure things stay this way, we are constantly working with high level experts on research and new developments. Furthermore, we are always close to our customers – thanks to our global manufacturing and service network. See for yourself, why our transformers make a difference!

 

Explore our worldwide transformer references

 

Green Transformers with ester insulation

Reliable power transmission from New Jersey to New York City

Make use of our services

For your convenience, we have assembled relevant downloads as well as details of support contacts below.

Transformer-Training

Free Basic Transformer-Training

Watch our training to understand the functionality, setup and operation of power transformers. Our training explains the transformer principle and gives an overview about different transformer types as well as their components and information on their operation and ageing – including life extension measures.

Contact

Get in contact with our Customer Service

You can contact us 24/7.
We are looking forward for your call or online request.

Phone +49 180 524 70 00

News & Media

Stay up to date with our transformers


Our transformers, upcoming industry events and tradeshows – get the latest news here!