Introduction

Set the right course in product design

Finding the balance between social, economic and environmental factors is a challenge. Optimal use of resources throughout the entire development and production process begins in design, with the selection of the right materials, efficient material use and reduced emissions in the production and utilization phase. Thanks to our internal eco-design processes, and with the help of life-cycle analyses (LCAs), we manage environmental aspects throughout development, and influence all stages of our product life cycles. And since environmentally friendly products are more economical, our customers also benefit.

Siemens has the necessary products and is one of the few companies worldwide that can develop complete solutions.

Dr. Michael Prange, Manager of German Water Partnership

The "Product Eco Excellence" Program

Our "Product Eco Excellence" program ensures that our products are safe, presenting no danger to humans and the environment. We know the footprint of our products and are constantly working to keep material and energy consumption as low as possible. Read on to learn more about chemical management, dealing with critical materials, and the environmental footprint of Siemens products.

Product Eco Excellence

Our program and minimize goals by 2020 to minimise the environmental impact of Siemens products

Chemical management

Handling chemicals at Siemens

A multitude of substances are used to manufacture products. Siemens ensures that both humans and the environment are protected from the harmful effects of these substances. We even exceed legal requirements in avoiding of these substances. In addition, Siemens utilizes a globally standardized directory in which substances to be declared for each product, including legally prohibited substances, are listed.

image

We know what’s in our products

Transparency regarding the nature and quantity of substances in products is becoming increasingly important. Especially when reusing or recycling materials, all contents must be known. Through proactive management of chemicals, Siemens guarantees compliance with internal policies as well as the requirements of our customers regarding substance declaration. We actively involve our suppliers in order to implement legal requirements, such as REACH (Registration, Evaluation, Authorization and Restriction of Chemicals) and RoHS (Restriction of Hazardous Substances), reliably.

Click here for a list of all declarable substances
LoDS-List

Ecological footprint

Making the footprint visible

Siemens determines the environmental footprint of products using life-cycle analyses (LCAs). These are used to analyze and optimize the environmental impact of our products, and they encompass all stages of the product lifecycle – from development to the application phase. Based on this information, we create Environmental Product Declarations (EPDs) for our customers, thus ensuring the necessary transparency of contents and environmental impact of Siemens products.

Shedding more light on the turbine

Critical materials

Plan for the scarcity of tomorrow’s resources, today

Over 10,000 materials and substances go into our products and services. The selection of materials used for product development is of great importance. Such decisions impact future business risks such as scarcity of resources, legal requirements and environmental damage. Siemens employs a valuation method which helps product developers evaluate the critical potential of materials and take them early into consideration during product development.

Critical Materials

image

Beryllium

Critical material due to toxic hazards and availability risks

Typical industrial applications include contact materials, alloying agents for beryllium copper, and X-ray machines.

image

Cobalt

Critical material due to toxic hazards and availability risks

Typical industrial applications include use in magnetic materials, superalloys, corrosion- and wear-resistant alloys, catalysts and electroplating.

image

Niobium

Critical material due to availability risks

Typical industrial applications include use in superconductors, superconducting magnets, superalloys, magnetic materials, corrosion- and wear-resistant alloys, catalysts and electroplating.

image

Cadmium

Critical material due to toxic hazards

Typical industrial applications include use in batteries as well as accumulators, alloys, solders, semiconductors and electroplating.

image

Neodymium (representative for rare earth)

Critical material due to availability risks

Typical industrial applications include magnetic materials in generators, motors, optical glasses and lasers.

image

Tungsten

Critical material due to availability risks

Typical industrial applications include superalloys, heavy metal alloys, catalysts, electrodes, in scanning tunneling microscopy and in diagnostic radiology.

image

Platinum (representative for platinum-group metals)

Critical material due to availability risks

Typical industrial applications include catalysts, electrodes, magnetic materials and in thermocouples and resistance thermometers.

image

Lead

Critical material due to toxic hazards

Typical industrial applications include use in batteries as well as accumulators, radiation shields, lead glass, electrodes, solders and special brass.