Skip to main content

Process Device Library ขับเคลื่อนโดย Actemium Schweiz

Actemium Schweiz AG is an innovative company that automates industrial processes sustainably and effectively and supports its customers in expanding their efficiency. The company plans, installs, and maintains innovative solutions in the field of electrical, automation and IT technology for networked industrial and process automation as well as in the areas of robotics, process, and system planning. Actemium also optimizes project management: intelligent planning, efficient implementation, and a holistic structure.

ทำไม PDL?

The Process Device Library is a cross-industry PLC library. It is used to set up automation and process control systems for areas such as heating, ventilation, air conditioning (HVAC), process industry, life science and food.


PDL was developed for the TIA Portal with S7-1500 and ET200 SP controllers. The enclosed Step 7 library contains all the I&C functions for the process industry and building automation. A connection to energy technology systems is also integrated. The core function is the automatic visualization of the components from the S7 program code. What sounds like a vision of the future has already been developed by our automation experts in Switzerland and Germany. The new Process Device Library not only ensures a standardized “look and feel” but also supports the automated generation of HMI and SCADA solutions.

ประโยชน์

  • User Experience, Engineering Efficiency, Cross-industry, Easy to Engineer
  • Features, Maintenance & Commissioning, Standardized devices, Industrie 4.0 Ready

ความสามารถที่โดดเด่น

สำรวจแหล่งข้อมูลและผลิตภัณฑ์ที่เกี่ยวข้อง

ข้อมูลและแหล่งข้อมูลเพิ่มเติม

เงื่อนไขเบื้องต้น