Skip to main content
Centralized, future-proof control of Belgium’s waterways
Reference

Future-proof control for Belgium’s waterway

De Vlaamse Waterweg modernized the 63 km Dessel-Turnhout-Schoten canal with EQUANS and Siemens. By centralizing 9 locks and 11 bridges, operations are safer, more reliable, and more efficient – meeting the demands of critical infrastructure 24/7.

Modernizing Belgian waterways

Belgium’s inland waterways move over 160 million tons of goods each year, yet with the increasing traffic, skippers face delays at bridges and locks. De Vlaamse Waterweg, which manages inland waterways in Flanders, set out to change this. Entrusting the system integrator EQUANS to equip the Dessel-Turnhout-Schoten canal with Siemens' advanced remote and centralized control technology, they achieved remarkable enhancements in speed and safety, revolutionizing and future-proofing the journey for countless boats.

Icon for 24/7 availability

Operations 24/7 without downtime

For critical infrastructure, availability is non-negotiable. The redundant SIMATIC S7-1518HF ensures continuous operations and enables centralized control from a single locatio – keeping waterways running around the clock.

Graphic with arrow up for: High efficiency

Enhanced safety and efficiency

Emergency controls must be reliable. With secure remote access and integration of camera feeds, operators have greater visibility than on-site - allowing them to manage faster more bridges and locks with the same workforce.

Icon for cyber security

High cybersecurity

Connecting third-party systems requires strong protection against cyberthreats. Using Siemens Flexible F-Link and SIMATIC ET 200SP, data is encrypted and safeguarded – ensuring the integrity of critical infrastructure.

Steering through the currents of change

Modernizing a canal that carries millions of tons of goods each year was no small task. De Vlaamse Waterweg, together with EQUANS and Siemens, had to address several critical challenges to ensure reliable, safe, and efficient operations for the future. Close cooperation and the right technology kept the project on course.

Future-Proof and Redundant Infrastructure

For critical infrastructure, reliability is non-negotiable. The canal system needed to be both future-proof and fully fault tolerant to guarantee uninterrupted service. Together with EQUANS, Siemens delivered a resilient backbone built on the redundant SIMATIC S7-1518HF which took over for the previous central PLC.

“If you follow these programming rules, you won't have to make any changes to the programming when you switch from a single central PLC to redundant PLCs – you'll only need to reconfigure. We relinked all the PLCs at 20 sites in a single night and everything worked right away.”

— James Brits, automation project manager at EQUANS

A surveillance camera is mounted on a pole in an outdoor area.

Safe remote control and compliance

Centralizing control meant tackling a complex mix of requirements: legislation on machine operations, safety, and cybersecurity demanded a solution that didn’t yet exist. Emergency procedures had to work redundantly both remotely and on site, while non-routable safety protocols made connectivity especially challenging. The breakthrough came with Siemens’ Flexible F-Link, combined with the SIMATIC ET 200SP – creating secure, encrypted communication over the existing fiber network. With integrated cameras, operators gained even greater visibility than before, giving them a steady hand at the helm, with greater visibility than ever before.

"Centralization has so many benefits: inland vessels no longer have to wait, and we can deploy our lock keepers better. We can control a lot more boats with the same number of people."
– Tom Verschuren, water technology expert at De Vlaamse Waterweg

Standardization and optimized maintenance

Operating a patchwork of different systems made maintenance difficult and disturbed the steady flow of operations. De Vlaamse Waterweg set out to create a unified infrastructure that would make operations more consistent and reliable. To achieve this, they chose to implement Siemens’ TIA Portal as the central engineering framework and integrated diagnostic tools, ensuring one standardized platform across all sites. This brought smoother processes, quicker maintenance, and long-term efficiency, along with cost savings and environmental gains through optimized water levels.

Construction site with a large building under construction, surrounded by various construction equipment and workers.

James Brits (EQUANS), Brecht Vandendoorent (Siemens) and Tom Verschuren (De Vlaamse Waterweg)

Charting the course ahead

The modernization of the Dessel-Turnhout-Schoten canal has already transformed daily operations – making them faster, safer, and more reliable. But for De Vlaamse Waterweg, this is only the beginning of a broader journey. Vessel waiting times have already been reduced significantly, and in the future, ships may even receive digital guidance similar to a “Google Maps for waterways”, with estimated arrival times and optimized navigation speeds. The long-term vision is to steer all Flemish waterways from three centralized control rooms in Evergem, Willebroek, and Hasselt. This next step will allow even better service with the same workforce and keep the region’s waterways on a steady course for decades to come.

Explore our products