Skip to main content

Accelerating sustainable food production in Singapore

Artisan Green, a leading indoor farming company, has partnered with Siemens to revolutionize sustainable food production in Singapore, combining advanced technology with a shared commitment to sustainability and the production of high-quality, locally grown produce.

The promise of indoor farming

Traditional farming methods are facing significant challenges due to a growing global population, increasing demand for fresh, nutritious food, unpredictable weather, and limited arable land. By leveraging Siemens' cutting-edge technology in automation and digitalization, Artisan Green's indoor farms will be equipped with an integrated management system that optimizes resource efficiency and minimizes environmental impact.

Siemens AG logo featuring a stylized 'S' in blue and white.

Moving towards a sustainable future

Unified digital platform

A single unified digital platform enables Artisan Green to seamlessly integrate and operate various food factory technologies alongside an ASRS that services a minimum of 5,500m² of grow beds.

Command-and-control module

A command-and-control module allows Artisan Green to digitally store its library of nutrient recipes and lighting profiles, each of which is designed to optimize plant yield and health at each stage of the plant’s life cycle.

Farm management

The Farm Management System automatically executes varies growth protocols for each crop, providing optimum transparency and control over all growing processes for improved consistency, resource efficiency and traceability.

End-to-end automation

The end-to-end automated farm system that reduces the reliance on manual labor also helps Artisan Green achieve greater resilience of production during situations such as a pandemic.

Crop planning and scheduling

The integration of crop planning and scheduling provides fresh food on demand while ensuring optimum utilization of all available grow beds.

Environmental benefits

Growing food closer to the end consumer decreases transportation emissions.

Clean produce

Automation that results in minimal human contact points helps Artisan Green provide consumers with the cleanest possible produce.

High-quality, locally grown produce

A green-colored wall with a textured pattern resembling a stone or brick surface.

Meeting the challenges of traditional farming

Singapore has embarked on a visionary path to build up the agri-food industry's capability and capacity to sustainably produce 30% of their nutritional needs by 2030. This ambitious goal is featured in the Singapore Green Plan 2030, aimed at creating a more resilient food future.

A sustainable future

In addition to the environmental benefits, indoor farming offers numerous advantages over conventional agriculture. By growing crops vertically in controlled environments, Artisan Green's indoor farms maximize land use efficiency, allowing for higher crop yields and reducing the need for pesticides and herbicides. This approach also eliminates the risk of soil erosion and contamination, ensuring the production of safe and nutritious food.

A green and white Siemens Artisan refrigerator with a door slightly open.
A green and white image of a product with a white background and a green border.

Technology integration for sustainable farming

Artisan Green's indoor farms will be equipped with Siemens' cutting-edge technology, including:

  • SIMATIC S7-1500 for optimum control of process and growing parameters
  • SIMATIC ET 200SP with Dali module for a granular adjustment of lighting intensity
  • Energy Manager for transparency and optimization of energy consumption

WinCC V8 and PM-Control to develop Overall Farm Management System including recipe control system for choosing the right cultivation program for individual crops

Artisan Green and Siemens collaboration

The collaboration between Artisan Green and Siemens represents a significant step forward in the field of sustainable food production. By combining the expertise and resources of both companies, this collaboration is poised to accelerate the adoption of indoor farming in Singapore. Together, Artisan Green and Siemens are reshaping the future of agriculture, creating a brighter and more sustainable food landscape for generations to come.

A person wearing a green shirt and a green hat is standing in front of a green wall.

เริ่มต้นการเดินทางของคุณ