Skip to main content
Denna sida visas med automatisk översättning. Visa på engelska istället?
FALLSTUDIE

Kyloptimering i AI-datacenter

Den globala efterfrågan på datorkraft växer. Nya, allt kraftfullare datacenter byggs ständigt. Den oöverträffade tillväxten av artificiell intelligens innebär att dessa datacenter måste vara mer effektiva och ekonomiska än någonsin tidigare.

Systems for special tasks

When designing and building its solutions, DCX Liquid Cooling Systems relies on the proven and trusted technology suppliers. The company uses our controllers, HMI panels and power supplies, which play important roles in the installations it builds.

DCX Liquid Cooling Systems' main customers are AI data processing centers, as well as the HPC, Hyperscale, Enterprise and Neocloud data centers. The company designs and manufactures Coolant Distribution Units (CDUs), complete direct cooling systems, immersion cooling and modular data centers.

The company also handles the deployment and installation of the cooling infrastructure. DCX Liquid Cooling Systems' direct cooling solutions have been installed by the data center operators in countries like Sweden, France, the United States, Turkey and Switzerland.

DCX Liquid Cooling Systems manufactures innovative liquid cooling systems based on proven technologies from Siemens and other companies.

The power distribution in an AI data center

In a data center, electricity flows from the power grid connection through the medium- and low-voltage switchgear, transformers, UPS modules and energy storage facilities, and then through the PDUs (Power Distribution Units) or busbars to the server racks. From there, it goes through the power supply units and VRM (Voltage Regulator Module) circuits to the CPUs, GPUs and TPUs that drive the data centers' computing power.

At the same time, most of the power used by the IT equipment is converted into heat.

“In the DCX system, specialized cold plates remove more than 80% of the heat from the server’s components. The heat flows through the Technology Cooling System loop to the FDU (Facility Coolant Distribution Unit) solutions. There it is transferred through a heat exchanger to a second loop, FWS (Facility Water System), which is isolated from the server room. FWS is responsible for further removing heat from the facility” – explains Maciej Szadkowski, Chief Technology Officer at DCX Liquid Cooling Systems. “This heat can then either be removed from by the dry coolers or used in a heat recovery system. We use also RDHX solutions, like rear door heat exchangers mounted at the back of the rack, because the remaining server components may still require limited air cooling. These cool air leaves the server and therefore limits its impact on the thermal conditions in the server room” – he adds.

As a result, it is possible to significantly reduce energy consumption. In a traditional data center, the cooling system can account for up to 40% of the total energy consumption.

“Of course, switching to the liquid cooling does not automatically mean 40% energy savings. Actual savings depend on several factors, including ambient temperature, cooling loop parameters and the amount of heat removed by liquid. The architecture used to recover the residual heat from the server room also plays a major role. Importantly, this heat can be used, among other things, to heat the swimming pools, greenhouses, and other facilities” – explains Tomasz Buk, Chief Executive Officer at DCX Liquid Cooling Systems.

DCX’s competitive advantage lies in its expertise and unconventional approach to technology development.