Skip to main content

Tidsresa med den digitala tvillingen

Simuleringsfunktioner har framstått som nyckeln till att anpassa sig till förändringarna i dagens miljö. Företag kan utnyttja denna teknik för att förbli konkurrenskraftiga genom att hantera branschutmaningar. Detta leder till verklig digital transformation där den digitala tvillingen spelar en nyckelroll.

Consider a production engineer discovering that production throughput has fallen short of expectations. Traditionally, diagnosing such issues requires combing through vast amounts of live production data, a daunting task that can take hours, or even days.

Eventually, the engineer uncovers the source of the disruption — a machine encountered a motor error over the weekend. The resulting downtime led to a production shortfall, jeopardizing quarterly targets.

Precious time is now focused on analyzing the problem to prevent it happening in the future — time that could have been dedicated to process optimization or energy efficiency projects.

As industry accelerates, companies need accurate diagnostics and the ability to develop and implement solutions as quickly as possible. However, traditional troubleshooting methods are reactive and time-consuming, making it difficult to implement proactive solutions.

Now, companies can use the comprehensive digital twin to transform how engineers analyze, optimize and predict product and production outcomes.

The comprehensive digital twin comprises a set of consistent digital models representing different aspects that can be used throughout the entire product lifecycle, the production lifecycle, and the supply chain. It seamlessly combines the real and digital worlds so engineers can make key decisions with higher confidence.

The digital twin also evolves along the lifecycle. It starts during the development of a product or the design and engineering of production, where designers can benefit from digital representations supporting simulation of behavioral aspects.

In the operational phase of a product or process, the physical asset and the digital twin coexist, generating value by creating a closed-loop connection that enables continuous optimization, predictive maintenance and informed design decisions for next-gen developments.

This enables engineers to refine and optimize products and production systems before investing in physical assets, reducing reliance on costly physical prototypes.

En digital tvillingvisualisering som visar sammankopplade system och dataflöde mellan fysiska och digitala miljöer.

Companies can expand their digital twin over time by integrating additional datasets, tailoring their models to specific needs as their experience grows.

As industries become more data-driven, leveraging a digital twin will allow manufacturers to gain deeper insights into production mechanics, resource allocation, and operational efficiency.

Due to these capabilities, the comprehensive digital twin can act as a sort of "time machine." It can replay and analyze the past, reflect the present and predict future states.

Initially, it enables the optimization of product and production system before investing in physical assets, reducing the need for physical prototypes and helps to avoid expensive failures.

During the operational phase, the comprehensive digital twin generates tremendous value by running "what-if" scenarios to predict performance and behavior.

It lays the foundation for making quick and confident decisions before taking action in the real world.

Digital twin deepens real-time insights

Manufacturers often struggle with real-time monitoring and data integration across their production systems. While traditional analytics focus on basic operational metrics, the digital twin offers a deeper level of insight by integrating diverse datasets into a unified framework.

Combining the digital and the real world with a comprehensive digital twin enables the seamless integration of the product and production lifecycles, including software and automation. It allows companies to design, simulate, test, optimize and validate products with the Digital Twin for Products.

Using the digital twin for production, it is possible to plan and optimize machines, lines and even complete factories and plants in the digital world.

The result is a continuous loop of optimization, from designing a product to realizing and optimizing it with performance data through the digital twin of performance.

Actionable insights that are derived from that data can facilitate confident decisions, aiming for productivity and process improvements, such as optimizing production scheduling.

This also means that machine malfunctions or failures in material delivery systems are identified and supplied to production engineers or technicians immediately. This real-time insight ensures that malfunctions receive immediate attention, minimizing costly downtime.

Rapid diagnostics and issue resolution

A Siemens employee stands in front of two computer monitors.

The digital twin can also "rewind" time, enabling engineers to diagnose product or production issues efficiently. On the production floor, engineers receive precise error messages pinpointing the time of failure and the affected machine rather than relying on inference from general metrics.

Consider a modern CNC machine equipped with advanced automation and connectivity. If a vibration warning is triggered on one of its cutting spindles, the operator is alerted immediately, prompting an investigation into the cause.

Using the digital twin, the operator can review the vibration warning within an immersive 3D environment, pinpointing the exact moment excessive vibrations occurred.

Fast-forwarding and rewinding the digital twin replay, the operator can analyze key events — such as the start of cutting with a new tool — and compare performance across different spindles.

Suppose one spindle experiences significantly higher torque levels during the cutting operation, indicating an anomaly in the workpiece properties.

By identifying this issue early, engineers can make informed decisions on corrective actions, reducing downtime and improving machine reliability.

Additionally, historical data analysis through the digital twin provides manufacturers with invaluable insights into recurring issues.

If a particular component frequently fails due to overheating, engineers can design alternative configurations, modify cooling processes, or incorporate predictive maintenance alerts to mitigate future risks.

Simulation for proactive optimization

Beyond diagnostics, the digital twin offers unparalleled predictive capabilities. It can predict future states to make the right decisions at the right time.

By leveraging simulation, engineers can forecast future machine performance, evaluate potential process modifications and mitigate risks before they materialize.

For instance, electric vehicle manufacturers use simulation to refine battery designs, assessing expected range, thermal performance and packaging efficiency.

Engineers can rapidly test design iterations, selecting the most optimal configuration without the constraints of physical prototyping.

In another case, wind turbine manufacturers use digital twin models to simulate operational conditions across various geographic locations. These simulations provide detailed insights into aerodynamic performance, energy output fluctuations, and the impact of environmental variables such as wind speed and temperature.

By forecasting turbine efficiency under diverse conditions, manufacturers can optimize blade designs and maintenance schedules to maximize energy generation.

Intelligent, agile and resilient

The digital win supports a dynamic, data-driven approach to product development and production management.

By empowering engineers with real-time insights, historical analysis, and predictive simulations, the digital twin reduces costly downtime and enhances overall production agility.

Through closed-loop optimization, companies can continuously refine product offerings and production processes using real-world performance data.

In the evolving industrial landscape, the comprehensive digital twin enables engineers to engage in a form of time travel — using insights from the past, present, and future to drive efficiency, sustainability and competitiveness in an increasingly complex industrial world.

June 2025

Relaterat innehåll

Digital enterprise

Harness the power of Industry 4.0 and accelerate your digital transformation.

En kvinna som står med en bärbar dator framför en logotyp som representerar det digitala företaget.