Skip to main content

Manufacturing and development location Amberg

At the Amberg site, two plants and two development units manufacture and develop products and solutions for the global market.

At the Amberg site, two plants and two development units manufacture and develop products and solutions for the global market. With the SIMATIC S7 control family and the SIMATIC HMI operating and monitoring systems, which roll off the production line at the Electronics Works Amberg (EWA), Siemens occupies a leading position worldwide. The device factory (GWA) manufactures products for industrial switching technology such as SIRIUS (switching and protecting consumers such as motors). In addition, circuit breakers for industrial applications, infrastructure, and buildings are developed at the site.

The multi-award-winning site uses state-of-the-art IT and manufacturing technology, making it the blueprint for the digital factory of the future. Customers and partners can gain an insight into this at “The Impulse” visitor center, which opened in 2021 and where digital technologies, concepts, and automation solutions for the autonomous factory are developed and presented.

Address

Fertigungs- und Entwicklungsstandort Amberg

Werner-von-Siemens-Straße 48-52
92224 Amberg

Tel: +49 9621 963-0

The Siemens Customer Service Center gladly provides additional contacts at:

0800 50 90 100

Monday through Friday, 8:00 a.m. to 5:00 p.m. This number is free from German landlines, but charges may apply via mobile networks

Contact

Operations Management Hans-Peter Scharl mailto:bettina.popp@siemens.com

Press Contact Bernhard Lott

Human Resources Department Ramona Grosser

Training and Dual Study Programs (SPE) online.ausbildung.spe@siemens.com

Pracovné miesta a kariéra v spoločnosti Siemens

Každý deň sa pýtame, ako môžeme zlepšiť život ľudí. Pomôžete nám vytvoriť dôležité riešenia do budúcnosti?

Usmievajúca sa žena s kučeravými vlasmi v modrej košeli v kancelárskom prostredí

Ďalšie informácie

The image shows a person standing in front of a large window with a view of a city skyline at night.

Digital transformation of an electronics plant

The Siemens electronics plant in Amberg relies on smart production data and future technologies for efficient manufacturing.

Traja usmievajúci sa ľudia stojaci spolu na tyrkysovom pozadí, pričom každý z nich rukami vytvára tvar srdca.

Vzdelávacie a duálne študijné programy

Objavte svoje príležitosti v spoločnosti Siemens.

Továreň Siemens v Erlangene dňa 10. decembra 2021 v Erlangene, Nemecko. Muž s notebookom sleduje robota.

Inovácia – pre lepšiu budúcnosť

V spoločnosti Siemens sa nápady stávajú inováciami. To pomáha našim zákazníkom pri transformácii odvetví, ktoré tvoria chrbticu nášho hospodárstva.

Fotografia Berlína v noci

O spoločnosti Siemens v Nemecku

Siemens — z Nemecka, pre Nemecko a svet: S približne 85 000 zamestnancami a niekoľkými tisíckami stážistov je Siemens jedným z najväčších súkromných zamestnávateľov a školiacich spoločností v Nemecku.